1.5.2 Wi-Fi provisioning System Service Configuration
The Wi-Fi Provisioning System Service library should be configured through MHC(MPLAB Harmony Configurator). The following figure shows the MHC configuration window for configuring the Wi-Fi Provisioning System Service and a brief description of various configuration options.
The Wi-Fi Provisioning System Service library MHC menu provide option to enable required Wi-Fi Provisioning methods base on user application requirements. User can select Command line , Socket mode and HTTP as shown in below diagram.

Configuration Options:
- WiFi Configuration Stored At ?
The Wi-Fi Provisioning System Service provide the two option to user to store the WiFi Configuration.
NVM :
The Wi-Fi Provisioning System Service store the WiFi Configuration into NVM using it's internal framework.
WiFi Configuration Stored at NVM Address(Program Flash memory):
- NVM Address for storing Wi-Fi Configuration.
- User can change this configuration value with program flash memory page aligned address.
- The Wi-Fi Provisioning System Service by defult reserve 4KB from user provide NVM address for storing Wi-Fi Configuration.
- User has to make sure the NVM address(Program Flash memory) page is not overwritten by application code.
Save Configuration in the NVM(Program flash memory):
- Indicates the Wi-Fi configuration storing in the NVM.
- This configuration is only valid when "Enable Wi-Fi Provisioning service" is enabled.
User :
- The Wi-Fi Provisioning System Service don't store the WiFi Configuration into any memory.
- The Wi-Fi Provisioning System generate the application callback using WiFi service with message type SYS_WIFI_PROVCONFIG for user to store and manage the WiFi Configuration as per their choice.
Wi-Fi Provisioning Methods
Command Line(CLI):
- Enable/Disable Wi-Fi Provision using command line.
HTTP pages:
- Enable/Disable Wi-Fi Provision using HTTP pages(webpage).
- HTTP Socket Number:
- User configuration for HTTP Server Socket.
- Defult port number is 80.
TCP socket:
- Enable/Disable Wi-Fi Provision using TCP Socket.
- TCP Socket Number:
- User configuration for TCP Server Socket.
- Defult port number is 6666. TCP Socket port number is used by Mobile Applicaiton and JSON.