4.23.4 static __inline__ uint8_t _crc_ibutton_update
static __inline__ uint8_t _crc_ibutton_update(uint8_t __crc, uint8_t __data)
Optimized Dallas (now Maxim) iButton 8-bit CRC calculation.
Polynomial: x^8 + x^5 + x^4 + 1 (0x8C) Initial value: 0x0
See http://www.maxim-ic.com/appnotes.cfm/appnote_number/27
The following is the equivalent functionality written in C.
uint8_t _crc_ibutton_update(uint8_t crc, uint8_t data) { uint8_t i; crc = crc ^ data; for (i = 0; i < 8; i++) { if (crc & 0x01) crc = (crc >> 1) ^ 0x8C; else crc >>= 1; } return crc; }