4.180.6 sleep.h
/* Copyright (c) 2002, 2004 Theodore A. Roth Copyright (c) 2004, 2007, 2008 Eric B. Weddington Copyright (c) 2005, 2006, 2007 Joerg Wunsch All rights reserved. Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met: * Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer. * Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution. * Neither the name of the copyright holders nor the names of contributors may be used to endorse or promote products derived from this software without specific prior written permission. THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* $Id$ */ #ifndef _AVR_SLEEP_H_ #define _AVR_SLEEP_H_ 1 #include <avr/io.h> #include <stdint.h> /** \file */ /** \defgroup avr_sleep <avr/sleep.h>: Power Management and Sleep Modes \code #include <avr/sleep.h>\endcode Use of the \c SLEEP instruction can allow an application to reduce its power comsumption considerably. AVR devices can be put into different sleep modes. Refer to the datasheet for the details relating to the device you are using. There are several macros provided in this header file to actually put the device into sleep mode. The simplest way is to optionally set the desired sleep mode using \c set_sleep_mode() (it usually defaults to idle mode where the CPU is put on sleep but all peripheral clocks are still running), and then call \c sleep_mode(). This macro automatically sets the sleep enable bit, goes to sleep, and clears the sleep enable bit. Example: \code #include <avr/sleep.h> ... set_sleep_mode(<mode>); sleep_mode(); \endcode Note that unless your purpose is to completely lock the CPU (until a hardware reset), interrupts need to be enabled before going to sleep. As the \c sleep_mode() macro might cause race conditions in some situations, the individual steps of manipulating the sleep enable (SE) bit, and actually issuing the \c SLEEP instruction, are provided in the macros \c sleep_enable(), \c sleep_disable(), and \c sleep_cpu(). This also allows for test-and-sleep scenarios that take care of not missing the interrupt that will awake the device from sleep. Example: \code #include <avr/interrupt.h> #include <avr/sleep.h> ... set_sleep_mode(<mode>); cli(); if (some_condition) { sleep_enable(); sei(); sleep_cpu(); sleep_disable(); } sei(); \endcode This sequence ensures an atomic test of \c some_condition with interrupts being disabled. If the condition is met, sleep mode will be prepared, and the \c SLEEP instruction will be scheduled immediately after an \c SEI instruction. As the intruction right after the \c SEI is guaranteed to be executed before an interrupt could trigger, it is sure the device will really be put to sleep. Some devices have the ability to disable the Brown Out Detector (BOD) before going to sleep. This will also reduce power while sleeping. If the specific AVR device has this ability then an additional macro is defined: \c sleep_bod_disable(). This macro generates inlined assembly code that will correctly implement the timed sequence for disabling the BOD before sleeping. However, there is a limited number of cycles after the BOD has been disabled that the device can be put into sleep mode, otherwise the BOD will not truly be disabled. Recommended practice is to disable the BOD (\c sleep_bod_disable()), set the interrupts (\c sei()), and then put the device to sleep (\c sleep_cpu()), like so: \code #include <avr/interrupt.h> #include <avr/sleep.h> ... set_sleep_mode(<mode>); cli(); if (some_condition) { sleep_enable(); sleep_bod_disable(); sei(); sleep_cpu(); sleep_disable(); } sei(); \endcode */ /* Define an internal sleep control register and an internal sleep enable bit mask. */ #if defined(SLEEP_CTRL) /* XMEGA devices */ #define _SLEEP_CONTROL_REG SLEEP_CTRL #define _SLEEP_ENABLE_MASK SLEEP_SEN_bm #define _SLEEP_SMODE_GROUP_MASK SLEEP_SMODE_gm #elif defined(SLPCTRL) /* New xmega devices */ #define _SLEEP_CONTROL_REG SLPCTRL_CTRLA #define _SLEEP_ENABLE_MASK SLPCTRL_SEN_bm #define _SLEEP_SMODE_GROUP_MASK SLPCTRL_SMODE_gm #elif defined(SMCR) #define _SLEEP_CONTROL_REG SMCR #define _SLEEP_ENABLE_MASK _BV(SE) #elif defined(__AVR_AT94K__) #define _SLEEP_CONTROL_REG MCUR #define _SLEEP_ENABLE_MASK _BV(SE) #elif !defined(__DOXYGEN__) #define _SLEEP_CONTROL_REG MCUCR #define _SLEEP_ENABLE_MASK _BV(SE) #endif /* Special casing these three devices - they are the only ones that need to write to more than one register. */ #if defined(__AVR_ATmega161__) #define set_sleep_mode(mode) \ do { \ MCUCR = ((MCUCR & ~_BV(SM1)) | ((mode) == SLEEP_MODE_PWR_DOWN || (mode) == SLEEP_MODE_PWR_SAVE ? _BV(SM1) : 0)); \ EMCUCR = ((EMCUCR & ~_BV(SM0)) | ((mode) == SLEEP_MODE_PWR_SAVE ? _BV(SM0) : 0)); \ } while(0) #elif defined(__AVR_ATmega162__) \ || defined(__AVR_ATmega8515__) #define set_sleep_mode(mode) \ do { \ MCUCR = ((MCUCR & ~_BV(SM1)) | ((mode) == SLEEP_MODE_IDLE ? 0 : _BV(SM1))); \ MCUCSR = ((MCUCSR & ~_BV(SM2)) | ((mode) == SLEEP_MODE_STANDBY || (mode) == SLEEP_MODE_EXT_STANDBY ? _BV(SM2) : 0)); \ EMCUCR = ((EMCUCR & ~_BV(SM0)) | ((mode) == SLEEP_MODE_PWR_SAVE || (mode) == SLEEP_MODE_EXT_STANDBY ? _BV(SM0) : 0)); \ } while(0) /* For xmegas, check presence of SLEEP_SMODE<n>_bm and define set_sleep_mode accordingly. */ #elif defined(__AVR_XMEGA__) #define set_sleep_mode(mode) \ do { \ _SLEEP_CONTROL_REG = ((_SLEEP_CONTROL_REG & ~(_SLEEP_SMODE_GROUP_MASK)) | (mode)); \ } while(0) /* For everything else, check for presence of SM<n> and define set_sleep_mode accordingly. */ #else #if defined(SM2) #define set_sleep_mode(mode) \ do { \ _SLEEP_CONTROL_REG = ((_SLEEP_CONTROL_REG & ~(_BV(SM0) | _BV(SM1) | _BV(SM2))) | (mode)); \ } while(0) #elif defined(SM1) #define set_sleep_mode(mode) \ do { \ _SLEEP_CONTROL_REG = ((_SLEEP_CONTROL_REG & ~(_BV(SM0) | _BV(SM1))) | (mode)); \ } while(0) #elif defined(SM) #define set_sleep_mode(mode) \ do { \ _SLEEP_CONTROL_REG = ((_SLEEP_CONTROL_REG & ~_BV(SM)) | (mode)); \ } while(0) #else #error "No SLEEP mode defined for this device." #endif /* if defined(SM2) */ #endif /* #if defined(__AVR_ATmega161__) */ /** \ingroup avr_sleep Put the device in sleep mode. How the device is brought out of sleep mode depends on the specific mode selected with the set_sleep_mode() function. See the data sheet for your device for more details. */ #if defined(__DOXYGEN__) /** \ingroup avr_sleep Set the SE (sleep enable) bit. */ extern void sleep_enable (void); #else #define sleep_enable() \ do { \ _SLEEP_CONTROL_REG |= (uint8_t)_SLEEP_ENABLE_MASK; \ } while(0) #endif #if defined(__DOXYGEN__) /** \ingroup avr_sleep Clear the SE (sleep enable) bit. */ extern void sleep_disable (void); #else #define sleep_disable() \ do { \ _SLEEP_CONTROL_REG &= (uint8_t)(~_SLEEP_ENABLE_MASK); \ } while(0) #endif /** \ingroup avr_sleep Put the device into sleep mode. The SE bit must be set beforehand, and it is recommended to clear it afterwards. */ #if defined(__DOXYGEN__) extern void sleep_cpu (void); #else #define sleep_cpu() \ do { \ __asm__ __volatile__ ( "sleep" "\n\t" :: ); \ } while(0) #endif #if defined(__DOXYGEN__) /** \ingroup avr_sleep Put the device into sleep mode, taking care of setting the SE bit before, and clearing it afterwards. */ extern void sleep_mode (void); #else #define sleep_mode() \ do { \ sleep_enable(); \ sleep_cpu(); \ sleep_disable(); \ } while (0) #endif #if defined(__DOXYGEN__) /** \ingroup avr_sleep Disable BOD before going to sleep. Not available on all devices. */ extern void sleep_bod_disable (void); #else #if defined(BODS) && defined(BODSE) #ifdef BODCR #define BOD_CONTROL_REG BODCR #else #define BOD_CONTROL_REG MCUCR #endif #define sleep_bod_disable() \ do { \ uint8_t tempreg; \ __asm__ __volatile__("in %[tempreg], %[mcucr]" "\n\t" \ "ori %[tempreg], %[bods_bodse]" "\n\t" \ "out %[mcucr], %[tempreg]" "\n\t" \ "andi %[tempreg], %[not_bodse]" "\n\t" \ "out %[mcucr], %[tempreg]" \ : [tempreg] "=&d" (tempreg) \ : [mcucr] "I" _SFR_IO_ADDR(BOD_CONTROL_REG), \ [bods_bodse] "i" (_BV(BODS) | _BV(BODSE)), \ [not_bodse] "i" (~_BV(BODSE))); \ } while (0) #endif #endif /*@}*/ #endif /* _AVR_SLEEP_H_ */