4.190.21 int vfprintf
int vfprintf(FILE *__stream, const char *__fmt, va_list
__ap)
vfprintf is the central facility of the
printf family of functions. It outputs values to
stream under control of a format string passed in
fmt. The actual values to print are passed as a variable argument
list ap.
vfprintf returns the number of characters written to
stream, or EOF in case of an error. Currently,
this will only happen if stream has not been opened with write
intent.
The format string is composed of zero or more directives: ordinary
characters (not %), which are copied unchanged to the output stream;
and conversion specifications, each of which results in fetching zero or more subsequent
arguments. Each conversion specification is introduced by the %
character. The arguments must properly correspond (after type promotion) with the
conversion specifier. After the %, the following appear in
sequence:
-
Zero or more of the following flags:
-
#The value should be converted to an "alternate form". For c, d, i, s, and u conversions, this option has no effect. For o conversions, the precision of the number is increased to force the first character of the output string to a zero (except if a zero value is printed with an explicit precision of zero). For x and X conversions, a non-zero result has the string `0x' (or `0X' for X conversions) prepended to it. -
0(zero) Zero padding. For all conversions, the converted value is padded on the left with zeros rather than blanks. If a precision is given with a numeric conversion (d, i, o, u, i, x, and X), the 0 flag is ignored. -
-A negative field width flag; the converted value is to be left adjusted on the field boundary. The converted value is padded on the right with blanks, rather than on the left with blanks or zeros. A - overrides a 0 if both are given. -
' ' (space) A blank should be left before a positive number produced by a signed conversion (d, or i).
-
+A sign must always be placed before a number produced by a signed conversion. A + overrides a space if both are used.
-
-
An optional decimal digit string specifying a minimum field width. If the converted value has fewer characters than the field width, it will be padded with spaces on the left (or right, if the left-adjustment flag has been given) to fill out the field width.
-
An optional precision, in the form of a period . followed by an optional digit string. If the digit string is omitted, the precision is taken as zero. This gives the minimum number of digits to appear for d, i, o, u, x, and X conversions, or the maximum number of characters to be printed from a string for
sconversions. -
An optional
lorhlength modifier, that specifies that the argument for the d, i, o, u, x, or X conversion is a"long int"rather thanint. Thehis ignored, as"short int"is equivalent toint. -
A character that specifies the type of conversion to be applied.
The conversion specifiers and their meanings are:
-
diouxXThe int (or appropriate variant) argument is converted to signed decimal (d and i), unsigned octal (o), unsigned decimal (u), or unsigned hexadecimal (x and X) notation. The letters "abcdef" are used for x conversions; the letters "ABCDEF" are used for X conversions. The precision, if any, gives the minimum number of digits that must appear; if the converted value requires fewer digits, it is padded on the left with zeros. -
pThevoid *argument is taken as an unsigned integer, and converted similarly as a%#xcommand would do. -
cTheintargument is converted to an"unsigned char", and the resulting character is written. -
sThe"char *"argument is expected to be a pointer to an array of character type (pointer to a string). Characters from the array are written up to (but not including) a terminating NUL character; if a precision is specified, no more than the number specified are written. If a precision is given, no null character need be present; if the precision is not specified, or is greater than the size of the array, the array must contain a terminating NUL character. -
%A%is written. No argument is converted. The complete conversion specification is "%%". -
eEThe double argument is rounded and converted in the format"[-]d.ddde±dd"where there is one digit before the decimal-point character and the number of digits after it is equal to the precision; if the precision is missing, it is taken as 6; if the precision is zero, no decimal-point character appears. An E conversion uses the letter'E'(rather than'e') to introduce the exponent. The exponent always contains two digits; if the value is zero, the exponent is 00. -
fFThe double argument is rounded and converted to decimal notation in the format"[-]ddd.ddd", where the number of digits after the decimal-point character is equal to the precision specification. If the precision is missing, it is taken as 6; if the precision is explicitly zero, no decimal-point character appears. If a decimal point appears, at least one digit appears before it. -
gGThe double argument is converted in stylefore(orForEforGconversions). The precision specifies the number of significant digits. If the precision is missing, 6 digits are given; if the precision is zero, it is treated as 1. Styleeis used if the exponent from its conversion is less than -4 or greater than or equal to the precision. Trailing zeros are removed from the fractional part of the result; a decimal point appears only if it is followed by at least one digit. -
SSimilar to thesformat, except the pointer is expected to point to a program-memory (ROM) string instead of a RAM string.
In no case does a non-existent or small field width cause truncation of a numeric field; if the result of a conversion is wider than the field width, the field is expanded to contain the conversion result.
Since the full implementation of all the mentioned features becomes fairly
large, three different flavours of vfprintf() can be selected using linker options.
The default vfprintf() implements all the mentioned
functionality except floating point conversions. A minimized version of vfprintf() is available that only implements the
very basic integer and string conversion facilities, but only the #
additional option can be specified using conversion flags (these flags are parsed
correctly from the format specification, but then simply ignored). This version can be
requested using the following compiler options:
If the full functionality including the floating point conversions is required, the following options should be used:
- Limitations:
-
-
The specified width and precision can be at most 255.
-
- Notes:
-
-
For floating-point conversions, if you link default or minimized version of vfprintf(), the symbol
? will be output and double argument will be skiped. So you output below will not be crashed. For default version the width field and the "pad to left" ( symbol minus ) option will work in this case. -
The
hhlength modifier is ignored (charargument is promouted toint). More exactly, this realization does not check the number ofhsymbols. -
But the
lllength modifier will to abort the output, as this realization does not operatelonglongarguments. -
The variable width or precision field (an asterisk
*symbol) is not realized and will to abort the output.
-