3.1.2 Low-Voltage Programming (LVP) Mode
1’, the Low-Voltage ICSP Programming
entry is enabled. To disable the Low-Voltage ICSP mode, the LVP bit must be programmed
to ‘0’. This can only be done while in the High-Voltage Entry mode.- MCLR is brought to VIL.
- A 32-bit key sequence is
presented on ICSPDAT and clocked by ICSPCLK. The Least Significant bit (LSb) of
the pattern is a ‘don’t care
X’. The Program/Verify mode entry pattern detect hardware verifies only the first 31 bits of the sequence and the last clock is required before the pattern detect goes active.
The key sequence is a specific 32-bit pattern, ‘32’h4d434850’ (more
easily remembered as MCHP in ASCII). The device will enter Program/Verify mode only if
the sequence is valid. The MSb of the Most Significant Byte (MSB) must be shifted in
first. Once the key sequence is complete, MCLR must be held at
VIL for as long as Program/Verify mode is to be maintained. For
Low-Voltage Programming timing, see Figure 3-3 and
Figure 3-4.
To enter LVP mode, the MSb of the Most Significant nibble must be shifted in first. This differs from entering the key sequence on some other device families.