2.5 Xplained Pro Standard Extension Header

The PIC32CZ CA8x/CA9x Curiosity Ultra development board has two Xplained Pro compatible interfaces that enable the use of existing expansion boards. Each interface consists of a dual-row, 30-pin, 100 mil, 90-degree extension male header, while Xplained Pro extensions have their female counterparts. The extension headers can be used to connect a variety of Xplained Pro extension boards or to access the pins of the target MCU directly.

Note: All pins are not always connected.

The Pinout description for the Xplained Pro Standard Extension Header1 and Header 2 are listed in the following tables.

Note: Due to a component footprint error, the pin-out of the External Power Connector (J101) is not compatible with the standard for extension boards. If an extender board is used that requires this header, an adapter must be used. See the schematic section of this document for the pinout of J101.
Table 2-4. EXT 1 Header Pinout
Pin numberNameDescriptionPort
1ID_EXT1Communication line to the ID chip on an extension boardConnected to PKOB4
2GNDGround-
3ADC0(+)Analog-to-digital converter (ADC), alternatively positive part of differential ADCPA18
4ADC0(-)Analog-to-digital converter, alternatively negative part of differential ADCPA17
5GPIO1General purpose I/OPB25
6GPIO2General purpose I/OPB26
7PWMH1High-Side PWMPB10
8PWML1Low-Side PWMPB11
9GPIO3General purpose I/OPA7
10GPIO4General purpose I/OPC24
11SDA2Data line for I2C interface. Always implemented, bus typePC0
12SCL2Clock line for I2C interface. Always implemented, bus type.PC1
13RX2Receiver line of target device UARTPC7
14TX2Transmitter line of target device UART.PC4
15SS2SPI Select or General purpose I/OPC10
16MOSIHost Out Client In (MOSI) line of serial peripheral interface. Always implemented, bus type.PC8
17MISOHost In Client Out (MISO) line of serial peripheral interface. Always implemented, bus type.PC11
18SCK2Clock for serial peripheral interface. Always implemented, bus typePC9
19GNDGround–
20VCCPower for extension boards (3.3V)–
Table 2-5. EXT 2 Header Pinout
Pin numberNameDescriptionPort/Pin
1ID_EXT2Communication line to the ID chip on an extension boardConnected to PKOB4
2GNDGround–
3ADC1(+)Analog-to-digital converter, alternatively positive part of differential ADCPA14
4ADC1(-)Analog-to-digital converter, alternatively negative part of differential ADCPA13
5GPIO5General purpose I/OPB27
6GPIO6General purpose I/OPB28
7PWMH2High-Side PWMPA22
8PWML2Low-Side PWMPA23
9GPIO7General purpose I/OPA8
10GPIO8General purpose I/OPE10
11SDA2Data line for I2C interface. Always implemented, bus typePC25
12SCL2Clock line for I2C interface. Always implemented, bus type.PC26
13RX2Receiver line of target device UARTPC22
14TX2Transmitter line of target device UART.PC21
15SS3SPI Client Select or General purpose I/OPC14
16MOSIHost Out Client In (MOSI) line of serial peripheral interface. Always implemented, bus type.PC12
17MISOHost In Client Out (MISO) line of serial peripheral interface. Always implemented, bus type.PC15
18SCK2Clock for serial peripheral interface. Always implemented, bus typePC13
19GNDGround–
20VCCPower for extension boards (3.3V)–