25.6.2.5 Clock/Calendar (Mode 2)

When the RTC Operating Mode bits in the Control A register (CTRLA.MODE) are written to 0x2, the counter operates in Clock/Calendar mode. See the RTC Block Diagram (Mode 2 — Clock/Calendar) figure in the Block Diagram from Related Links. When the RTC is enabled, the counter increments on every 0-to-1 transition of CLK_RTC_CNT. The selected clock source and RTC prescaler must be configured to provide a 1 Hz clock to the counter for correct operation in this mode.

The time and date can be read from or written to the Clock Value register (CLOCK) in a 32-bit time/date format. Time is represented as:

  • Seconds
  • Minutes
  • Hours

Hours can be represented in either 12- or 24-hour format, selected by the Clock Representation bit in the Control A register (CTRLA.CLKREP). This bit can be changed only while the RTC is disabled.

The date is represented in this form:

  • Day as the numeric day of the month (starting at 1)
  • Month as the numeric month of the year (1 = January, 2 = February and so on)
  • Year as a value from 0x00 to 0x3F. This value must be added to a user-defined reference year. The reference year must be a leap year (2016, 2020, etc). Example: the year value, 0x2D, added to a reference year, 2016, represents the year 2061.

The RTC increments until it reaches the top value of 23:59:59 December 31 of year value 0x3F, then wraps to 00:00:00 January 1 of year value 0x00. This sets the Overflow Interrupt flag in the Interrupt Flag Status and Clear registers (INTFLAG.OVF).

The clock value is continuously compared with the 32-bit Alarm registers (ALARMn, n=0–1). When an alarm match occurs, the Alarm n Interrupt flag in the Interrupt Flag Status and Clear registers (INTFLAG.ALARMn, n=0..1) is set on the next 0-to-1 transition of CLK_RTC_CNT. For example, for a 1 Hz clock counter, it means the Alarm 0 Interrupt flag is set with a delay of 1s after the alarm match occurs.

A valid alarm match depends on the setting of the Alarm Mask Selection bits in the Alarm n Mask register (MASKn.SEL). These bits determine which time/date fields of the clock and alarm values are valid for comparison and which are ignored.

If the Clear on Match bit in the Control A register (CTRLA.MATCHCLR) is set, the counter is cleared on the next counter cycle when an alarm match with ALARMn occurs. This allows the RTC to generate periodic interrupts or events with longer periods than would be possible with the prescaler events only (see Periodic Intervals from Related Links).
Note: When CTRLA.MATCHCLR is ‘1’, INTFLAG.ALARMn and INTFLAG.OVF will both be set simultaneously on an alarm match with ALARMn.