Programming the Device
This section describes the steps to program the PolarFire SoC device with the job file using FlashPro Express. Download the job file from the following link: https://github.com/polarfire-soc/sev-kit-reference-design/releases/download/v2022.09/MPFS_SEV_KIT_DESIGN_2022_09.zip
Follow these steps:
- Connect a micro-USB to J5 from the host PC and start the FlashPro Express software from its installation directory.
- Select New or New Job Project from FlashPro Express Job from the Project menu to create a new job project, see the following figure.
Figure . New FlashPro Express Project - In the New Job Project from FlashPro Express Job dialog box, enter the following:
- Programming job file: Click Browse and navigate to the location where the job file is located and select the file.
- FlashPro Express job project location: Select Browse and navigate to the location where you want to save the project.
- Click Open. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears. Confirm that a programmer number appears in the Programmer field. If it does not, check the board connections and click Refresh/Rescan Programmers.
- Click RUN to program the device. When the device is programmed successfully, a RUN PASSED status is displayed.
- Close FlashPro Express (Project > Exit).
- Power-cycle the board.