6 Known Issues
| # | ID | Description | Device(s) |
|---|---|---|---|
| 1 | M8BTL-1431 | Installing the library on Mac from the content manager requires a restart of MPLAB X to allow the library to appear in the resource window | All Devices |
| 2 | M8BTL-1433 | Configuring a device with less than 16KB will require a limited command
set. Example: Write Support, Erase Support, Checksum Support, Basic Verification | All Devices |
| 3 | M8BTL-1511 | Some versions of the USART driver require the Weak Pull-up to be enabled for
both the Tx and Rx pins. Workaround: If UBHA is failing to connect to an AVR device and your pins are correctly configured. Consider turning on the Weak Pull-ups. | AVR |
| 4 | M8BTL-1513 | Slower clock speeds will cause the bootloader to respond slowly to some
commands. Workaround: It is recommended to use a high frequency clock setting. Calculations like checksum will time out in UBHA if the processing time is too slow. | All Devices |
| 5 | M8BTL-1436 | Optimization level 2 is set by default anytime MCC
refreshes. Workaround: There is no workaround to this other than setting the desired optimization setting after you click the generate button or update a UI setting. | All Devices |
| 6 | CC8SCRIP-7249 | PIC16F devices may fail to program if an external clock is
used. Workaround: The workaround presented is actually to set the clock values to the desired configuration for the application you are writing. The behavior has been fixed but the default generation on some device will not program the bootloader. The bootloader will work with the High Frequency Internal Oscillator. | PIC16F |