4.13.2 SPI with Control and Status Registers
4.13.2.1 Introduction
The Serial Peripheral Interface (SPI) module is a serial interface useful for communicating with other peripheral or microcontroller devices. These peripheral devices may be serial EEPROMs, shift registers, display drivers, Analog-to-Digital (A/D) converters, etc.
4.13.2.2 Supported Device Families
| ATmega32x |
4.13.2.3 Required header files:
#include "mcc_generated_files/spi/spi[X].h"
4.13.2.4 Module Documentation
4.13.2.4.1 SPI0
This header file provides API prototypes for the SPI0 driver.
Module description
This header file provides API prototypes for the SPI0 driver.
Data structures
struct SPI_INTERFACE
Defines an object for SPI_INTERFACE functions.
Functions
void SPI0_Initialize (void)
Initializes the SPI0 module.
void SPI0_Deinitialize (void)
Deinitializes the SPI0 module.
bool SPI0_Open (uint8_t spiConfigIndex)
Enables the SPI0 module with the configurations passed as the parameter. See spi0_config_names_t for the available configurations.
void SPI0_Close (void)
Closes the active configuration of the SPI0 module.
void SPI0_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI0_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI0_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI0_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI0_IsRxReady (void)
Checks if the SPI0 module is ready to read data.
bool SPI0_IsTxReady (void)
Checks if the SPI0 is ready to write data.
Function Documentation
SPI0_BufferExchange()
void SPI0_BufferExchange (void * bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
| in,out | *bufferData |
Buffer address of the data to be exchanged |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI0_BufferRead()
void SPI0_BufferRead (void * bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
| out | *bufferData |
Buffer address of the data to be read |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI0_BufferWrite()
void SPI0_BufferWrite (void * bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
| in | *bufferData |
Buffer address of the data to be written |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI0_ByteExchange()
uint8_t SPI0_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
| byteData |
Byte to be written |
Received data byte |
SPI0_ByteRead()
uint8_t SPI0_ByteRead (void )
Receives one byte using the SPI protocol.
| None. |
Received data byte |
SPI0_ByteWrite()
void SPI0_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
| byteData |
Byte to be written |
None. |
SPI0_Close()
void SPI0_Close (void )
Closes the active configuration of the SPI0 module.
| None. |
None. |
SPI0_Deinitialize()
void SPI0_Deinitialize (void )
Deinitializes the SPI0 module.
| None. |
None. |
SPI0_Initialize()
void SPI0_Initialize (void )
Initializes the SPI0 module.
| None. |
None. |
SPI0_IsRxReady()
bool SPI0_IsRxReady (void )
Checks if the SPI0 module is ready to read data.
| None. |
| True |
SPI0 module is ready to read data |
| False |
SPI0 module is not ready to read data |
SPI0_IsTxReady()
bool SPI0_IsTxReady (void )
Checks if the SPI0 is ready to write data.
| None. |
| True |
SPI0 module is ready to write data |
| False |
SPI0 module is not ready to write data |
SPI0_Open()
bool SPI0_Open (uint8_t spiConfigIndex)
Enables the SPI0 module with the configurations passed as the parameter. See spi0_config_names_t for the available configurations.
| spiConfigIndex |
Configuration index |
| True |
SPI0 module is enabled successfully with the chosen configuration |
| False |
SPI0 module is already open with another configuration |
4.13.2.4.2 SPI1
This header file provides API prototypes for the SPI1 driver.
Module description
This header file provides API prototypes for the SPI1 driver.
Data structures
struct SPI_INTERFACE
Defines an object for SPI_INTERFACE functions.
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI1_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
bool SPI1_IsTxReady (void)
Checks if the SPI1 is ready to write data.
void SPI1_RxCompleteCallbackRegister (void(*rxCompleteCallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer receive in Interrupt mode.
void SPI1_TxCompleteCallbackRegister (void(*txCompleteCallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer transmit in Interrupt mode.
void SPI1_Receive_ISR (void)
Interrupt Service Routine (ISR) with receive interrupt RXIF for the SPI1 module.
void SPI1_Transmit_ISR (void)
ISR with transmit interrupt TXIF for the SPI1 module.
void SPI1_ISR (void)
ISR for the SPI1 module.
Function Documentation
SPI1_BufferExchange()
void SPI1_BufferExchange (void * bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
| in,out | *bufferData |
Buffer address of the data to be exchanged |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI1_BufferRead()
void SPI1_BufferRead (void * bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
| out | *bufferData |
Buffer address of the data to be read |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI1_BufferWrite()
void SPI1_BufferWrite (void * bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
| in | *bufferData |
Buffer address of the data to be written |
| in | bufferSize |
Size of the data in bytes |
None. |
SPI1_ByteExchange()
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
| byteData |
Byte to be written |
Received data byte |
SPI1_ByteRead()
uint8_t SPI1_ByteRead (void )
Receives one byte using the SPI protocol.
| None. |
Received data byte |
SPI1_ByteWrite()
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
| byteData |
Byte to be written |
None. |
SPI1_Close()
void SPI1_Close (void )
Closes the active configuration of the SPI1 module.
| None. |
None. |
SPI1_Deinitialize()
void SPI1_Deinitialize (void )
Deinitializes the SPI1 module.
| None. |
None. |
SPI1_Initialize()
void SPI1_Initialize (void )
Initializes the SPI1 module.
| None. |
None. |
SPI1_ISR()
void SPI1_ISR (void )
ISR for the SPI1 module.
| None. |
None. |
SPI1_IsRxReady()
bool SPI1_IsRxReady (void )
Checks if the SPI1 module is ready to read data.
| None. |
| True |
SPI1 module is ready to read data |
| False |
SPI1 module is not ready to read data |
SPI1_IsTxReady()
bool SPI1_IsTxReady (void )
Checks if the SPI1 is ready to write data.
| None. |
| True |
SPI1 module is ready to write data |
| False |
SPI1 module is not ready to write data |
SPI1_Open()
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
| spiConfigIndex |
Configuration index |
| True |
SPI1 module is enabled successfully with the chosen configuration |
| False |
SPI1 module is already open with another configuration |
SPI1_Receive_ISR()
void SPI1_Receive_ISR (void )
Interrupt Service Routine (ISR) with receive interrupt RXIF for the SPI1 module.
| None. |
None. |
SPI1_RxCompleteCallbackRegister()
void SPI1_RxCompleteCallbackRegister (void(*)(void) rxCompleteCallbackHandler)
Sets the callback function to be executed at the completion of data transfer receive in Interrupt mode.
| Pointer |
to the function to be executed |
None. |
SPI1_Transmit_ISR()
void SPI1_Transmit_ISR (void )
ISR with transmit interrupt TXIF for the SPI1 module.
| None. |
None. |
SPI1_TxCompleteCallbackRegister()
void SPI1_TxCompleteCallbackRegister (void(*)(void) txCompleteCallbackHandler)
Sets the callback function to be executed at the completion of data transfer transmit in Interrupt mode.
| Pointer |
to the function to be executed |
None. |
4.13.2.4.3 SPI
This header file provides API prototypes for the SPI module in Polling and Interrupt mode.
Module description
This header file provides API prototypes for the SPI module in Polling and Interrupt mode.
This header file provides type definitions for the SPI module operation in Polling mode.
This header file provides type definitions for the SPI module operation in Interrupt mode.
Data structures
struct SPI_INTERFACE
Defines an object for SPI_INTERFACE functions.
Enumerations
enum spi_status_t { SPI_RESET = 0x00U, SPI_IDLE = 0x81U, SPI_BUSY = 0x42U }
Enumeration for the different states of the SPI module.
enum spi_transfer_type_t { SPI_READ = 0x00U, SPI_WRITE = 0x81U, SPI_EXCHANGE = 0X42U }
Enumeration for the different transfer types of the SPI module.
Enumeration Type Documentation
spi_status_t
enum enum spi_status_t
Enumeration for the different states of the SPI module.
The enum values are chosen with a specific bit pattern to make sure no error happens in case a single bit changes.
| SPI_RESET |
SPI module is in Reset state |
| SPI_IDLE |
SPI module is ready to use |
| SPI_BUSY |
SPI module is in use |
spi_transfer_type_t
enum enum spi_transfer_type_t
Enumeration for the different transfer types of the SPI module.
The enum values are chosen with a specific bit pattern to make sure no error happens in case a single bit changes.
| SPI_READ |
SPI module is performing a read operation |
| SPI_WRITE |
SPI module is performing a write operation |
| SPI_EXCHANGE |
SPI module is performing a exchange operation |
4.13.2.5 Class Documentation
4.13.2.5.1 spi_configuration_t Struct Reference
#include <spi_interrupt_types.h>
Public Attributes
Member Data Documentation
The documentation for this struct was generated from the following files:
source/source-files/
source/source-files/
spcr
uint8_t spcr
spsr
uint8_t spsr
4.13.2.5.2 spi_descriptor_t Struct Reference
#include <spi_interrupt_types.h>
Public Attributes
uint8_t * buffer
size_t bufferLength
Member Data Documentation
The documentation for this struct was generated from the following file:
source/source-files/
buffer
uint8_t* buffer
bufferLength
size_t bufferLength
status
spi_status_t status
transferType
spi_transfer_type_t transferType
4.13.2.5.3 SPI_INTERFACE Struct Reference
Defines an object for SPI_INTERFACE functions.
Detailed Description
Defines an object for SPI_INTERFACE functions.
SPI Driver prototypes struct.
SPI driver interface object.
#include <spi_interface_interrupt.h>
Public Attributes
void(* Initialize )(void)
void(* Deinitialize )(void)
bool(* Open )(uint8_t spiConfigIndex)
void(* Close )(void)
void(* BufferExchange )(void *bufferData, size_t bufferSize)
void(* BufferRead )(void *bufferData, size_t bufferSize)
void(* BufferWrite )(void *bufferData, size_t bufferSize)
uint8_t(* ByteExchange )(uint8_t byteData)
uint8_t(* ByteRead )(void)
void(* ByteWrite )(uint8_t byteData)
bool(* IsRxReady )(void)
bool(* IsTxReady )(void)
void(* RxCompleteCallbackRegister )(void(*callbackHandler)(void))
void(* TxCompleteCallbackRegister )(void(*callbackHandler)(void))
Member Data Documentation
The documentation for this struct was generated from the following files:
source/source-files/
source/source-files/
BufferExchange
void(* BufferExchange
BufferRead
void(* BufferRead
BufferWrite
void(* BufferWrite
ByteExchange
uint8_t(* ByteExchange
ByteRead
uint8_t(* ByteRead
ByteWrite
void(* ByteWrite
Close
void(* Close
Deinitialize
void(* Deinitialize
Initialize
void(* Initialize
IsRxReady
bool(* IsRxReady
IsTxReady
bool(* IsTxReady
Open
bool(* Open
RxCompleteCallbackRegister
void(* RxCompleteCallbackRegister
TxCompleteCallbackRegister
void(* TxCompleteCallbackRegister
4.13.2.6 File Documentation
4.13.2.6.1 source/source-files/spi0_polling.c File Reference
#include "../spi0.h" #include "../spi_polling_types.h"
Functions
void SPI0_Initialize (void)
Initializes the SPI0 module.
void SPI0_Deinitialize (void)
Deinitializes the SPI0 module.
bool SPI0_Open (uint8_t spiConfigIndex)
Enables the SPI0 module with the configurations passed as the parameter. See spi0_config_names_t for the available configurations.
void SPI0_Close (void)
Closes the active configuration of the SPI0 module.
void SPI0_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI0_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI0_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI0_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI0_IsRxReady (void)
Checks if the SPI0 module is ready to read data.
bool SPI0_IsTxReady (void)
Checks if the SPI0 is ready to write data.
Variables
const struct SPI_INTERFACE SPI0
static const spi_configuration_t spi0_configuration []
Variable Documentation
SPI0
const struct SPI_INTERFACE SPI0
Initial value:
= {
.Initialize = SPI0_Initialize,
.Deinitialize = SPI0_Deinitialize,
.Open = SPI0_Open,
.Close = SPI0_Close,
.BufferExchange = SPI0_BufferExchange,
.BufferWrite = SPI0_BufferWrite,
.BufferRead = SPI0_BufferRead,
.ByteExchange = SPI0_ByteExchange,
.ByteWrite = SPI0_ByteWrite,
.ByteRead = SPI0_ByteRead,
.IsRxReady = SPI0_IsRxReady,
.IsTxReady = SPI0_IsTxReady,
.RxCompleteCallbackRegister = NULL,
.TxCompleteCallbackRegister = NULL
}
spi0_configuration
const spi_configuration_t spi0_configuration[][static]
Initial value:
= {
{ 0x53, 0x0 }
}
4.13.2.6.2 source/source-files/spi0_polling.h File Reference
#include "../system/utils/compiler.h" #include "spi_interface.h"
Functions
void SPI0_Initialize (void)
Initializes the SPI0 module.
void SPI0_Deinitialize (void)
Deinitializes the SPI0 module.
bool SPI0_Open (uint8_t spiConfigIndex)
Enables the SPI0 module with the configurations passed as the parameter. See spi0_config_names_t for the available configurations.
void SPI0_Close (void)
Closes the active configuration of the SPI0 module.
void SPI0_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI0_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI0_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI0_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI0_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI0_IsRxReady (void)
Checks if the SPI0 module is ready to read data.
bool SPI0_IsTxReady (void)
Checks if the SPI0 is ready to write data.
Enumerations
enum spi0_configuration_name_t { SPI0_DEFAULT }
Variables
const struct SPI_INTERFACE SPI0
Enumeration Type Documentation
spi0_configuration_name_t
enum spi0_configuration_name_t
| SPI0_DEFAULT |
Variable Documentation
SPI0
const struct SPI_INTERFACE SPI0
4.13.2.6.3 source/source-files/spi1_interrupt.c File Reference
#include "../spi1.h" #include "../spi_interrupt_types.h"
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI1_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI1_IsTxReady (void)
Checks if the SPI1 is ready to write data.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
void SPI1_RxCompleteCallbackRegister (void(*rxCompleteCallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer receive in Interrupt mode.
void SPI1_ISR (void)
ISR for the SPI1 module.
ISR (SPI1_STC_vect)
Variables
const struct SPI_INTERFACE SPI1
static void(* SPI1_RxCompleteCallback )(void)
static spi_descriptor_t spi1_descriptor
static const spi_configuration_t spi1_configuration []
Function Documentation
ISR()
ISR (SPI1_STC_vect )
Variable Documentation
SPI1
const struct SPI_INTERFACE SPI1
Initial value:
= {
.Initialize = SPI1_Initialize,
.Deinitialize = SPI1_Deinitialize,
.Open = SPI1_Open,
.Close = SPI1_Close,
.BufferExchange = SPI1_BufferExchange,
.BufferWrite = SPI1_BufferWrite,
.BufferRead = SPI1_BufferRead,
.ByteExchange = SPI1_ByteExchange,
.ByteWrite = SPI1_ByteWrite,
.ByteRead = SPI1_ByteRead,
.IsTxReady = SPI1_IsTxReady,
.IsRxReady = SPI1_IsRxReady,
.RxCompleteCallbackRegister = SPI1_RxCompleteCallbackRegister,
.TxCompleteCallbackRegister = NULL
}
spi1_configuration
const spi_configuration_t spi1_configuration[][static]
Initial value:
= {
{ 0x53, 0x0 }
}
spi1_descriptor
spi_descriptor_t spi1_descriptor[static]
Initial value:
= {
.buffer = NULL,
.bufferLength = 0U,
.status = SPI_RESET
}
SPI1_RxCompleteCallback
void(* SPI1_RxCompleteCallback) (void)[static]
4.13.2.6.4 source/source-files/spi1_interrupt.h File Reference
#include "../system/utils/compiler.h" #include "spi_interface.h"
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte using the SPI protocol.
uint8_t SPI1_ByteRead (void)
Receives one byte using the SPI protocol.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
bool SPI1_IsTxReady (void)
Checks if the SPI1 is ready to write data.
void SPI1_RxCompleteCallbackRegister (void(*rxCompleteCallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer receive in Interrupt mode.
void SPI1_TxCompleteCallbackRegister (void(*txCompleteCallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer transmit in Interrupt mode.
void SPI1_Receive_ISR (void)
Interrupt Service Routine (ISR) with receive interrupt RXIF for the SPI1 module.
void SPI1_Transmit_ISR (void)
ISR with transmit interrupt TXIF for the SPI1 module.
void SPI1_ISR (void)
ISR for the SPI1 module.
Enumerations
enum spi1_configuration_name_t { SPI1_DEFAULT }
Variables
const struct SPI_INTERFACE SPI1
Enumeration Type Documentation
spi1_configuration_name_t
enum spi1_configuration_name_t
| SPI1_DEFAULT |
Variable Documentation
SPI1
const struct SPI_INTERFACE SPI1
4.13.2.6.5 source/source-files/spi_interface_interrupt.h File Reference
#include <stdint.h> #include <stdbool.h> #include <stddef.h>
Data structures
struct SPI_INTERFACE
Defines an object for SPI_INTERFACE functions.
4.13.2.6.6 source/source-files/spi_interface_polling.h File Reference
#include <stdint.h> #include <stdbool.h> #include <stddef.h>
Data structures
struct SPI_INTERFACE
Defines an object for SPI_INTERFACE functions.
4.13.2.6.7 source/source-files/spi_interrupt_types.h File Reference
Data structures
struct spi_descriptor_t
struct spi_configuration_t
Enumerations
enum spi_status_t { SPI_RESET = 0x00U, SPI_IDLE = 0x81U, SPI_BUSY = 0x42U }
Enumeration for the different states of the SPI module.
enum spi_transfer_type_t { SPI_READ = 0x00U, SPI_WRITE = 0x81U, SPI_EXCHANGE = 0X42U }
Enumeration for the different transfer types of the SPI module.
Detailed Description
SPI Type Definitions Header File
4.13.2.6.8 source/source-files/spi_polling_types.h File Reference
Data structures
struct spi_configuration_t
Detailed Description
SPI Type Definitions Header File