4.1 Application Demo Setup
This section provides an overview about the hardware, software and related utility tools required for the demo setup.
Hardware Requirements
- Two Microchip RN4678 PICtail™/PICtail PLUS boards
- Two PIC18 Explorer Development boards with PIC18F87J11 PIMs mounted
- One of the following Microchip development tools for programming and
debugging:
- MPLAB REAL ICE™ in-circuit emulator
- MPLAB ICD 3
- PICkit™ 3
- Two power supplies – 9V/0.75A batteries
- 1 multi-strand (gauge > 20) wires with soldered female berg connector on one side and male berg connector on another end
Software/Utility Requirements
The application demo source code relating to this application note is written in an MPLAB X workspace project file and is available for download from the Microchip website. The code is compiled using the Microchip XC8 compiler v2.00 and MPLAB X IDE v3.05.
Use the precompiled RN4678_MCU18_Interface.X.production.hex file of
the demo or, if required, compile the RN4678_MCU18_Interface project
code. Ensure the compilation is successful. For additional information
on the source code, related files with description and call graph, refer to the
Appendix B: Source Code. From
MPLAB X, the user can generate call graphs related to specific functions of the demo
code.