4 ATWINC15x0 Configuration
The ATWINC15x0 firmware offers a set of configurable parameters that control its behavior. There is a set of APIs provided to the host MCU application to configure these parameters. The configuration APIs are categorized according to their functionality, into device, network and power saving parameters.
Any parameters left unset by the host MCU application use their default values assigned during the initialization of the ATWINC15x0 firmware. A host MCU application needs to configure its parameters when coming out of cold boot or when a specific configuration change is required.