1.11.1.16 ADCHS_EOSCallbackRegister Function
C
void ADCHS_EOSCallbackRegister (uintptr_t context)
Summary
Registers the function to be called from end of scan interrupt
Description
This function registers the callback function to be called from end of scan interrupt
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void ADCHS_Callback_Fn(uintptr_t context)
{
}
ADCHS_Initialize();
ADCHS_EOSCallbackRegister(ADCHS_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.