1.11.1.30 ADCHS_FilterxCallbackRegister Function
C
void ADCHS_FilterxCallbackRegister(ADCHS_DF_CALLBACK callback, uintptr_t context) // x - Filter number
Summary
Registers the function to be called from the ADC filter ready interrupt
Description
This function registers the callback function to be called from the ADC filter ready interrupt
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients). |
Returns
None.
Example
void ADCHS_Filter1_Callback_Fn(uintptr_t context)
{
uint16_t filter_data;
filter_data = ADCHS_Filter1DataGet();
}
ADCHS_Filter1CallbackRegister(ADCHS_Filter1_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.