1.11.1.17 ADCHS_DMASampleCountBaseAddrSet Function

C

void ADCHS_DMASampleCountBaseAddrSet(uint32_t baseAddr)

Summary

Registers the user-defined RAM address at which the DMA engine will start saving the current count of output samples

Description

Registers the user-defined RAM address at which the DMA engine will start saving the current count of output samples

Precondition

ADCHS_Initialize() must have been called first for the associated instance.

Parameters

Param Description
baseAddr Physical address of the user-defined RAM address

Returns

None.

Example

__COHERENT uint8_t adcSampleCntBuffer;
ADCHS_DMASampleCountBaseAddrSet((uint32_t)KVA_TO_PA(adcSampleCntBuffer));

Remarks

None