1.11.1.24 ADCHS_ComparatorxEventModeSet Function

C

void ADCHS_ComparatorxEventModeSet(ADCHS_CMP_EVENT_MODE eventMode) // x - Comparator number 

Summary

Sets the condition under which the comparator output becomes true

Description

Sets the condition under which the comparator output becomes true

Precondition

ADCHS_Initialize() must have been called first for the associated instance.

Parameters

Param Description
eventMode A logical OR of the following events: ADCHS_CMP_EVENT_MODE_IELOLO ADCHS_CMP_EVENT_MODE_IELOHI ADCHS_CMP_EVENT_MODE_IEHILO ADCHS_CMP_EVENT_MODE_IEHIHI ADCHS_CMP_EVENT_MODE_IEBTWN

Returns

None

Example

ADCHS_Comparator1EventModeSet(ADCHS_CMP_EVENT_MODE_IELOHI | ADCHS_CMP_EVENT_MODE_IEHIHI);

Remarks

None