1.11.1.15 ADCHS_CallbackRegister Function
C
void ADCHS_CallbackRegister (ADCHS_CHANNEL_NUM channel, ADCHS_CALLBACK callback, uintptr_t context)
Summary
Registers the function to be called from interrupt
Description
This function registers the callback function to be called from interrupt
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channel | Analog channel number |
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void ADCHS_Callback_Fn(ADCHS_CHANNEL_NUM channel, uintptr_t context)
{
}
ADCHS_Initialize();
ADCHS_CallbackRegister(ADCHS_CH0, ADCHS_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.