1.28.12.2 OTPC_WritePacket Function
C
otpc_error_code_t OTPC_WritePacket(const OTPC_NEW_PACKET *packet,
const uint32_t *payload,
uint16_t *headerAddress,
uint16_t *sizeWritten);
Summary
Perform an OTPC packet write.
Description
Create a new packet with the given payload. Returns the address of the packet and size written (in number of bytes).
Precondition
OTPC_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
packet | Pointer to the structure defining the packet attributes |
payload | Pointer to the address of new payload |
headerAddress | Address of the newly created packet(output)} |
sizeWritten | number of bytes written into the new packet |
Returns
otpc error code.
Example
OTPC_Initialize(); OTPC_WritePacket(&packet, &payload, &headerAddress, &sizeWritten);
Remarks
None