1.28.12.7 OTPC_HidePacket Function
C
otpc_error_code_t OTPC_HidePacket(uint16_t headerAddress);
Summary
Hides the packet
Description
Hides a packet with a given address. Attempting to read a hidden packet will return all zeros.
Precondition
OTPC_Initialize() function must have been called first and a valid packet should exist at the address.
Parameters
Param | Description |
---|---|
headerAddress | Address of the packet |
Returns
OTPC error code
Example
OTPC_Initialize(); OTPC_HidePacket(headerAddress);
Remarks
None