1.1.9.1 QMSPIx_Initialize Function

C

// x - Instance of the QMSPI peripheral

void QMSPIx_Initialize( void );

Summary

Initializes given instance of the QMSPI peripheral.

Description

This function initializes the given instance of the QMSPI peripheral as configured by the user.

Precondition

None.

Parameters

None.

Returns

None.

Example

QMSPI0_Initialize();