1.7.2.27 ADCHS_ComparatorxStatusGet Function

C

bool ADCHS_ComparatorxStatusGet(void)

Summary

Returns the Comparator status

Description

Returns the Comparator status. This API is generated when interrupt mode is disabled.

Precondition

ADCHS_Initialize() must have been called first for the associated instance.

Parameters

None

Returns

Returns Comparator status

Example

if (ADCHS_Comparator1StatusGet())
{

}

Remarks

None