1.7.2.25 ADCHS_ComparatorxAnalogInputIDGet Function
C
uint8_t ADCHS_ComparatorxAnalogInputIDGet(void) // x - Comparator number
Summary
Identifies the analog input for which the comparator event is generated
Description
Identifies the analog input for which the comparator event is generated
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
None
Returns
uint8_t - Analog input id for which the comparator event is generated
Example
uint8_t ain_id; ain_id = ADCHS_Comparator1AnalogInputIDGet();
Remarks
None