1.13.13.22 MCPWM_CallbackRegister Function
C
void MCPWM_CallbackRegister (MCPWM_CH_NUM channel, MCPWM_CH_CALLBACK callback, uintptr_t context)
Summary
Registers the function to be called from interrupt
Description
This function registers the callback function to be called from interrupt
Precondition
MCPWM_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channel | MCPWM channel number |
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void MCPWM_Callback_Fn(MCPWM_CH_STATUS status, uintptr_t context); MCPWM_Initialize(); MCPWM_CallbackRegister(MCPWM_CH_0, MCPWM_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.