1.13.13.4 MCPWM_SecondaryPeriodGet Function
C
uint16_t MCPWM_SecondaryPeriodGet (void)
Summary
Reads the period value of secondary time base generator
Description
This function reads the period value of secondary time base generator
Precondition
MCPWM_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
The MCPWM secondary time base period value
Example
uint16_t period; MCPWM_Initialize(); period = MCPWM_SecondaryPeriodGet();
Remarks
None