1.1.6.5 LEDx_DutyCycleMinSet Function

C

/* x = LED peripheral instance number */

void LEDx_DutyCycleMinSet(uint8_t min)

Summary

Specifies the minimum duty cycle value.

Description

When the current duty cycle is less than or equal to the min value the breathing apparatus holds the current duty cycle for the period specified by the field LD in register LED_DELAY

Precondition

None

Parameters

Param Description
min Minimum value of the duty cycle in LED breathing mode

Returns

None

Example

LED0_DutyCycleMinSet(50);

Remarks

None