1.27.9.15 MCANx_ErrorCountGet Function
C
void MCANx_ErrorCountGet(uint8_t *txErrorCount, uint8_t *rxErrorCount) // x - Instance of the MCAN peripheral
Summary
Returns the transmit and receive error count during transfer.
Precondition
MCANx_Initialize must have been called for the associated MCAN instance.
Parameters
Param | Description |
---|---|
txErrorCount | Transmit Error Count to be received |
rxErrorCount | Receive Error Count to be received |
Returns
None.
Example
uint8_t txErrorCount = 0; uint8_t rxErrorCount = 0; MCAN0_ErrorCountGet(&txErrorCount, &rxErrorCount);
Remarks
None.