1.24.4.6 CANx_MessageAbort Function
C
The prototype of CANx_MessageAbort() varies based on device family. Refer to the generated header file for the actual prototype to be used.
void CANx_MessageAbort(uint8_t fifoNum) // x - Instance of the CAN peripheral void CANx_MessageAbort(uint8_t fifoQueueNum) // x - Instance of the CAN peripheral void CANx_MessageAbort(CAN_MAILBOX_MASK mailboxMask) // x - Instance of the CAN peripheral
Summary
Abort request for a FIFO (or Mailbox).
Description
This routine aborts the transmitted message to FIFO (or Mailbox).
Precondition
CANx_Initialize must have been called for the associated CAN instance.
Parameters
Param | Description |
---|---|
fifoNum | FIFO number |
fifoQueueNum | If fifoQueueNum is 0 then Transmit Queue otherwise FIFO |
mailboxMask | Mailbox mask |
Returns
None
Example
CAN1_MessageAbort(0);
CAN0_MessageAbort(CAN_MAILBOX_0_MASK);
Remarks
None.