1.2.2.22 ADC_ChannelConversionStart Function
C
ADC_ChannelConversionStart(void)
Summary
Starts conversion on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API
Description
Starts conversion on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
None
Example
ADC_ChannelConversionStart();
Remarks
None