1.25.26.10 XDMACn_ChannelBlockLengthSet Function
C
// n is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral. void XDMACn_ChannelBlockLengthSet (XDMAC_CHANNEL channel, uint16_t length);
Summary
Sets the channel Block Length of a specific XDMAC Channel.
Description
This function sets the channel Block Length of the XDMAC channel. The length of the block is (BLEN+1) microblocks. Any ongoing transaction of the specified XDMAC channel will be aborted when this function is called.
Precondition
XDMAC should have been initialized by calling XDMACn_Initialize.
Parameters
Param | Description |
---|---|
channel | A specific XDMAC channel |
length | The number of microblocks of data |
Returns
None
Example
XDMAC_ChannelBlockLengthSet(XDMAC_CHANNEL_0, 16);
Remarks
None