1.25.26.12 XDMACn_ChannelResume Function

C

// n is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
void XDMACn_ChannelResume(XDMAC_CHANNEL channel)

Summary

This function Resumes the DMA channel

Description

The function Resumes the specified XDMAC channel. If the channel is already suspended, the channel operation resumes from where it previously stopped when the Resume command is detected. When the Resume command is issued before the channel is suspended, the next suspend action is skipped and the channel continues the normal operation.

Precondition

XDMAC should have been initialized by calling XDMACn_Initialize and channel should be enabled.

Parameters

Param Description
XDMAC_CHANNEL channel the particular channel to be Resumed

Returns

None.

Example

XDMAC_ChannelResume (XDMAC_CHANNEL_0);