1.30.15.27 RTC_Timer16PeriodGet Function
C
uint16_t RTC_Timer16PeriodGet ( void )
Summary
Get 16-bit timer period Value.
Description
This function returns the 16-bit timer period value which used to compare with the current counter value. This value will match the value that was set using the RTC_Timer16PeriodSet() function.
Precondition
RTC_Initialize must have been called for the associated RTC instance. The RTC peripheral should have been configured in 16-bit Timer Counter mode
Parameters
None.
Returns
The current 16-bit timer period value.
Example
uint16_t period = 0; RTC_Initialize(); RTC_Timer16PeriodSet(0xFFF); // period will have the same value is 0xFFF. period = RTC_Timer16PeriodGet();
Remarks
None.