1.29.7.3 DIVAS_DivUnsigned Function

C

uint32_t DIVAS_DivUnsigned( uint32_t numerator, uint32_t denominator)

Summary

This function uses the DIVAS peripheral to performs a unsigned 32-bit division.

Description

This function uses the DIVAS peripheral to perform a unsigned 32-bit division. The function takes a unsigned divisor and dividend and returns the quotient

Precondition

The peripheral should have been initialized by calling the DIVAS_Initialize() function once.

Parameters

Param Description
numerator This should contain the unsigned dividend.
denominator This should contain the unsigned divisor.

Returns

Returns quotient

Example

uint32_t dividend;
uint32_t divisor;
uint32_t quotient;

dividend = 10000;
divisor = 2000;

quotient = DIVAS_DivUnsigned(dividend, divisor)

Remarks

None.