1.30.16.14 TCx_Timer8bitCompareSet Function

C

/* x = TC instance number */
void TCx_Timer8bitCompareSet ( uint8_t compare );

Summary

Sets the compare value of a given timer channel.

Description

This function writes the compare value. When timer counter matches compare value, interrupt can be generated.

Precondition

TCx_TimerInitialize function must have been called first for the given channel.

Parameters

Param Description
compare compare value of the timer

Returns

None.

Example

TC0_TimerInitialize();
TC0_Timer8bitCompareSet(0xFul);

Remarks

This function is available only when TC timer mode is used by SYS_TIME module. SYS_TIME uses compare match interrupt to generate dynamic delay.