1.26.20.21 TCx_CHy_CaptureAGet Function
C
/* x = TC instance number, y= channel number */ /* 16 bit counter */ uint16_t TCx_CHy_CaptureAGet ( void ) /* 32 bit counter */ uint32_t TCx_CHy_CaptureAGet ( void )
Summary
Returns the Capture-A value.
Description
This function provides the Capture-A value that was stored when the selected event occurred on the input signal. The caller should call the TCx_CHy_CaptureAEventOccured function to identify if the Capture-A value has been updated by the selected signal event.
Precondition
TCx_CHy_TimerInitialize() function must have been called first for the given channel to configure channel in capture mode.
Parameters
None
Returns
Most recent Capture-A value. Type of return value varies with the bit width of the counter.
Example
16 bit counter
uint16_t capture; if (TC0_CH1_CaptureAEventOccured() == true) { capture = TC0_CH1_CaptureAGet(); }
32 bit counter
uint32_t capture; if (TC0_CH1_CaptureAEventOccured() == true) { capture = TC0_CH1_CaptureAGet(); }
Remarks
This function is applicable only for capture mode.