1.28.16.1 PWMx_Initialize Function
C
/* x = PWM instance number */ void PWMx_Initialize (void)
Summary
Initializes given instance of PWM peripheral
Description
This function initializes given instance of PWM periphral with the values configured in MCC GUI. This initializes all the selected channels of given peripheal in MCC GUI.
Precondition
MCC GUI should be configured with the right values.
Parameters
None.
Returns
None.
Example
PWM0_Initialize();
Remarks
This function must be called before any other PWM function is called. This function should only be called once during system initialization.