1.10.13.9 MCPWM_Initialize Function
C
void MCPWM_Initialize (void)
Summary
Initializes given instance of MCPWM peripheral
Description
This function initializes given instance of MCPWM peripheral with the values configured in MCC GUI. This initializes all the selected generators of given peripheral in MCC GUI.
Precondition
MCC GUI should be configured with the right values.
Parameters
None.
Returns
None.
Example
MCPWM_Initialize();
Remarks
This function must be called before any other MCPWM function is called. This function should only be called once during system initialization.