1.9.4.4 DMA_ChannelIsBusy Function

C

bool DMA_ChannelIsBusy ( DMA_CHANNEL channel )

Summary

The function returns the busy status of the channel.

Description

The function returns true if the specified channel is busy with a transfer. This function can be used to poll for the completion of transfer that was started by calling the DMA_ChannelTransfer() function. This function can be used as a polling alternative to setting a callback function and receiving an asynchronous notification for transfer notification.

Precondition

DMA should have been initialized by calling DMA_Initialize.

Parameters

Param Description
channel The DMA channel whose status needs to be checked.

Returns

True - The channel is busy with an on-going transfer.

False - The channel is not busy and is available for a transfer.

Example

// Wait while the channel is busy.
while(DMA_ChannelIsBusy (DMA_CHANNEL_0));

Remarks

None.