1.34.12.9 QSPIx_Write Function
C
// x - Instance of the QSPI peripheral
bool QSPIx_Write(void* pTransmitData, size_t txSize);
Summary
Write data on QSPI peripheral. This is used in SPI mode only.
Description
This function should be used to write "txSize" number of bytes on QSPI module. Data pointed by pTransmitData is transmitted.
Precondition
The QSPIx_Initialize function must have been called. Callback has to be registered using QSPIx_CallbackRegister API if the peripheral instance has been configured in Interrupt mode and transfer completion status needs to be communicated back to application via callback.
Parameters
Param | Description |
---|---|
*pTransmitData | Pointer to the data which has to be transmitted. if it isNULL, that means only data receiving is expected. For 9 to 15bit mode, data should be right aligned in the 16 bit memory location. |
txSize | Number of bytes to be transmitted. Always, size should begiven in terms of bytes. For example, if 5 16-bit data are to be transmitted, the transmit size should be 10 bytes. |
Returns
-
In Blocking mode:
-
API returns True once the transfer is complete. It returns False if txSize parameter is 0 and transmit data pointer is NULL.
-
-
In interrupt mode:
-
If previous buffer request is not completed and a new transfer request comes, then this API will reject the new request and will return "False".
-
Also, Same as blocking mode, It returns False if txSize parameter is 0 and transmit data pointer is NULL.
-
Example
uint8_t txBuffer[4]; size_t txSize = 4; bool reqAccepted; reqAccepted = QSPI0_Write(&txBuffer, txSize);
Remarks
Non-blocking interrupt mode configuration implementation of this function will be used by Harmony driver implementation APIs.