1.42.3.67 FLEXCOMx_TWI_ErrorGet Function
C
/* x = FLEXCOM instance number */
/* TWI master mode */
FLEXCOM_TWI_ERROR FLEXCOMx_TWI_ErrorGet(void)
Summary
Returns the TWI error that occurred on the bus.
Description
This function returns the TWI error that occurred on the bus. The function can be called to identify the error cause.
Precondition
FLEXCOMx_TWI_Initialize must have been called for the associated FLEXCOM TWI instance.
Parameters
None.
Returns
Returns error of type FLEXCOM_TWI_ERROR, identifying the error that has occurred.
Example
if(FLEXCOM0_TWI_ErrorGet() == FLEXCOM_TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. }
Remarks
None