3.28.16 Random Access Memory (RAM)
The Random Access Memory (RAM) module provides an interface to perform write and read on the device's Internal SRAM or External DRAM memory locations
Using The Library
The Internal SRAM or External DRAM memory locations can be read/written using the simple memcpy based Read and Write API's.
This PLIB is mainly used by Memory Driver when configured with File system for treating RAM as a media to store files.
The example code below demonstrates how to write and read from RAM location.
uint8_t buffer[256]; RAM_Write( (uint32_t *) buffer, 256, 0x20000000); RAM_Read( (uint32_t *) buffer, 256, 0x20000000);
Library Interface
Random Access Memory peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| RAM_Read | Reads length number of bytes from a given address in RAM |
| RAM_Write | Write length number of bytes to a given address in RAM |
| RAM_IsBusy | Returns the current status of RAM |
| RAM_ECC_StatusGet | Returns the current ECC status for the RAM. |
| RAM_ECC_SingleBitFaultInject |
Injects a single-bit fault at a specified RAM address. |
| RAM_ECC_InterruptHandler | Handles RAM ECC interrupts |
| RAM_ECC_Initialize | Enables ECC error detection interrupts for the RAM module. |
| RAM_ECC_FaultEnable | Enables fault injection for ECC in RAM. |
| RAM_ECC_FaultDisable | Disables fault injection for ECC in RAM. |
| RAM_ECC_FaultCaptureSyndromeGet | Returns the ECC fault syndrome value. |
| RAM_ECC_FaultCaptureParityGet | Returns the parity of the captured ECC fault. |
| RAM_ECC_FaultCaptureAddrGet | Returns the address of the captured ECC fault. |
| RAM_ECC_Enable | Enable the ECC functionality for the RAM. |
| RAM_ECC_DoubleBitFaultInject | Injects a double-bit fault at specified address. |
| RAM_ECC_Disable | Disable the ECC functionality for the RAM. |
| RAM_ECC_CallbackRegister | Enable the ECC functionality for the RAM. |