2.94.12 RAM_ECC_FaultCaptureAddrGet Function
C
uint32_t RAM_ECC_FaultCaptureAddrGet(void)
Summary
Returns the address of the captured ECC fault.
Description
This function returns the address where the last ECC fault was detected in the RAM, as stored in the MCRAMC_ERRCADR register.
Precondition
None
Parameters
None
Returns
returns the fault address
Example
uint32_t faultAddress; // Get the address of the captured ECC fault faultAddress = RAM_ECC_FaultCaptureAddrGet();