2.94.11 RAM_ECC_FaultCaptureParityGet Function
C
uint8_t RAM_ECC_FaultCaptureParityGet(void)
Summary
Returns the parity of the captured ECC fault.
Description
This function returns the parity value associated with the most recent ECC fault detected in the RAM.
Precondition
None
Parameters
None
Returns
parity value of ECC fault.
Example
uint8_t faultParity; // Get the parity value of the captured ECC fault faultParity = RAM_ECC_FaultCaptureParityGet();