3.32.7 ARM Cortex A Generic timer (GENERIC_TIMER)
The Generic Timer:
Provides a system counter, that measures the passing of time in real-time
Provides timers, that can assert a timer output signal after a period of time has passed.
The timers can be used as a count-up or count-down timers
Using The Library
Generic Timer plib implements uses the counter view of the generic timer, wherein it is used as 64 bit up-counter
Timer is initialized using GENERIC_TIMER_Initialize() function which configures the timer registers with values based on the MCC GUI settings for this plib
Timer can be started using GENERIC_TIMER_Start() function and stopped using GENERIC_TIMER_Stop() APIs
Timer period can be set using GENERIC_TIMER_PeriodSet() function
If a callback is registered using GENERIC_TIMER_CallbackRegister() function, when the timer period expires (i.e. when the interrupt occurs), the callback function will be executed
Library Interface
ARM Cortex A Generic timer peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| GENERIC_TIMER_Initialize | Initialize Generic Timer registers per user config |
| GENERIC_TIMER_CounterValueGet | Returns 64 bit counter value |
| GENERIC_TIMER_CounterFrequencyGet | Returns counter frequency |
| GENERIC_TIMER_Start | Start the Generic timer |
| GENERIC_TIMER_Stop | Stop Generic timer |
| GENERIC_TIMER_PeriodSet | Set the timer period value |
| GENERIC_TIMER_PeriodGet | Get the timer period value |
| GENERIC_TIMER_DelayMs | Delays processing for x milliseconds |
| GENERIC_TIMER_DelayUs | Delays processing for x microseconds |
| GENERIC_TIMER_CallbackRegister | Register callback for generic timer interrupt |
Data types and constants
| Name | Type | Description |
|---|---|---|
| GENERIC_TIMER_CALLBACK | Typedef | Generic Timer Interrupt Callback Function definition |