3.32.6 Flexible Serial Communication Controller (FLEXCOM)
A FLEXCOM can be configured in USART, SPI or TWI mode
USART Mode
This section provides interface to use the FLEXCOM peripheral in USART mode. The FLEXCOM USART PLIB can be configured in blocking, non-blocking or ring buffer mode.
Blocking mode
In blocking mode, the transfer APIs block until the requested data is transferred.
Non-blocking mode
In non-blocking mode the peripheral interrupt is enabled. The transfer API initiates the transfer and returns immediately. The transfer is then completed from the peripheral interrupt. Application can either use a callback to get notified when the transfer is complete or can use the IsBusy API to check the completion status.
Ring buffer mode
In ring buffer mode, the receiver is always enabled, and the received data is saved in the internal receive ring buffer, size of which can be configured using MCC. The application can use the API calls to read the data out from the ring buffer. APIs are provided to query the number of (unread) bytes available in the receive buffer, free space in the receive buffer and size of the receive buffer. Similarly, during transmission, the application data is deep copied into the internal transmit ring buffer, size of which can be configured using MCC. This allows the use of local buffers for data transmission. APIs are provided to query the free space in the transmit buffer, number of bytes pending transmission and the size of the transmit buffer. Additionally, application can enable notifications to get notified when n bytes are available in the receive buffer or when n bytes of free space is available in the transmit buffer. The APIs allow application to set the threshold levels for notification in both receive and transmit buffers. Further, application can also choose to enable persistent notifications, whereby the application is notified until the threshold condition is met.
In all the modes, library provides API to change the baud, parity, data width and the number of stop bits at run time.
Using The Library
Blocking Mode
#define RX_BUFFER_SIZE 10 char message[] = "FLEXCOM Example in blocking mode"; char receiveBuffer[RX_BUFFER_SIZE] = {0}; USART_ERROR errorStatus; char rxData = 0; int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Transmit buffer*/ FLEXCOM0_USART_Write(message, sizeof(message)); /* Wait for a character to be received */ while(FLEXCOM0_USART_ReceiverIsReady() == false); if(FLEXCOM0_USART_ErrorGet() == USART_ERROR_NONE) { /* Read a byte */ rxData = FLEXCOM0_USART_ReadByte(); } /* Receive buffer */ if (FLEXCOM0_USART_Read(receiveBuffer, RX_BUFFER_SIZE)) == false) { /* Read failed, get the error */ errorStatus FLEXCOM0_USART_ErrorGet(); /* Handle the error */ } else { /* Transmit the received buffer*/ FLEXCOM0_USART_Write(receiveBuffer, RX_BUFFER_SIZE); } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
Non-blocking Mode
#define RX_BUFFER_SIZE 10 char message[] = "**** Non-blocking Transfer with the interrupt ****\r\n\ **** Type 10 characters. The received characters are echoed back ****\r\n"; char messageError[] = "**** USART error occurred ****\r\n"; char receiveBuffer[RX_BUFFER_SIZE] = {0}; char echoBuffer[RX_BUFFER_SIZE+4] = {0}; bool errorStatus = false; bool writeStatus = false; bool readStatus = false; void APP_WriteCallback(uintptr_t context) { writeStatus = true; } void APP_ReadCallback(uintptr_t context) { if(FLEXCOM0_USART_ErrorGet() != USART_ERROR_NONE) { /* ErrorGet clears errors, set error flag to notify console */ errorStatus = true; } else { readStatus = true; } } int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Register callback functions and send start message */ FLEXCOM0_USART_WriteCallbackRegister(APP_WriteCallback, 0); FLEXCOM0_USART_ReadCallbackRegister(APP_ReadCallback, 0); FLEXCOM0_USART_Write(&message[0], sizeof(message)); while ( true ) { if(errorStatus == true) { /* Send error message to console */ errorStatus = false; FLEXCOM0_USART_Write(&messageError[0], sizeof(messageError)); } else if(readStatus == true) { /* Echo back received buffer and Toggle LED */ readStatus = false; echoBuffer[0] = '\n'; echoBuffer[1] = '\r'; memcpy(&echoBuffer[2], receiveBuffer,sizeof(receiveBuffer)); echoBuffer[RX_BUFFER_SIZE+2] = '\n'; echoBuffer[RX_BUFFER_SIZE+3] = '\r'; FLEXCOM0_USART_Write(&echoBuffer[0], sizeof(echoBuffer)); } else if(writeStatus == true) { /* Submit buffer to read user data */ writeStatus = false; FLEXCOM0_USART_Read(&receiveBuffer[0], sizeof(receiveBuffer)); } else { /* Repeat the loop */ ; } } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
Ring buffer Mode
uint8_t txBuffer[50]; uint8_t rxBuffer[10]; volatile uint32_t nBytesRead = 0; volatile bool txThresholdEventReceived = false; volatile bool rxThresholdEventReceived = false; void usartReadEventHandler(FLEXCOM_USART_EVENT event, uintptr_t context ) { uint32_t nBytesAvailable = 0; if (event == FLEXCOM_USART_EVENT_READ_THRESHOLD_REACHED) { /* Receiver should atleast have the thershold number of bytes in the ring buffer */ nBytesAvailable = FLEXCOM0_USART_ReadCountGet(); nBytesRead += FLEXCOM0_USART_Read((uint8_t*)&rxBuffer[nBytesRead], nBytesAvailable); } } void usartWriteEventHandler(FLEXCOM_USART_EVENT event, uintptr_t context ) { txThresholdEventReceived = true; } int main ( void ) { uint32_t nBytes = 0; /* Initialize all modules */ SYS_Initialize ( NULL ); /* Register a callback for write events */ FLEXCOM0_USART_WriteCallbackRegister(usartWriteEventHandler, (uintptr_t) NULL); /* Register a callback for read events */ FLEXCOM0_USART_ReadCallbackRegister(usartReadEventHandler, (uintptr_t) NULL); /* Print the size of the read buffer on the terminal */ nBytes = sprintf((char*)txBuffer, "RX Buffer Size = %d\r\n", (int)FLEXCOM0_USART_ReadBufferSizeGet()); FLEXCOM0_USART_Write((uint8_t*)txBuffer, nBytes); /* Print the size of the write buffer on the terminal */ nBytes = sprintf((char*)txBuffer, "TX Buffer Size = %d\r\n", (int)FLEXCOM0_USART_WriteBufferSizeGet()); FLEXCOM0_USART_Write((uint8_t*)txBuffer, nBytes); FLEXCOM0_USART_Write((uint8_t*)"Adding 10 characters to the TX buffer - ", sizeof("Adding 10 characters to the TX buffer - ")); /* Wait for all bytes to be transmitted out */ while (FLEXCOM0_USART_WriteCountGet() != 0); FLEXCOM0_USART_Write((uint8_t*)"0123456789", 10); /* Print the amount of free space available in the TX buffer. This should be 10 bytes less than the configured write buffer size. */ nBytes = sprintf((char*)txBuffer, "\r\nFree Space in Transmit Buffer = %d\r\n", (int)FLEXCOM0_USART_WriteFreeBufferCountGet()); FLEXCOM0_USART_Write((uint8_t*)txBuffer, nBytes); /* Let's enable notifications to get notified when the TX buffer is empty */ FLEXCOM0_USART_WriteThresholdSet(FLEXCOM0_USART_WriteBufferSizeGet()); /* Enable notifications */ FLEXCOM0_USART_WriteNotificationEnable(true, false); /* Wait for the TX buffer to become empty. Flag "txThresholdEventReceived" is set in the callback. */ while (txThresholdEventReceived == false); txThresholdEventReceived = false; /* Disable TX notifications */ FLEXCOM0_USART_WriteNotificationEnable(false, false); FLEXCOM0_USART_Write((uint8_t*)"Enter 10 characters. The received characters are echoed back. \r\n>", sizeof("Enter 10 characters. The received characters are echoed back. \r\n>")); /* Wait till 10 (or more) characters are received */ while (FLEXCOM0_USART_ReadCountGet() < 10); /* At-least 10 characters are available in the RX buffer. Read out into the application buffer */ FLEXCOM0_USART_Read((uint8_t*)rxBuffer, 10); /* Echo the received data */ FLEXCOM0_USART_Write((uint8_t*)rxBuffer, 10); /* Now demonstrating receiver notifications */ FLEXCOM0_USART_Write((uint8_t*)"\r\n Now turning on RX notifications \r\n>", sizeof("\r\n Now turning on RX notifications \r\n>")); /* For demonstration purpose, set a threshold value to receive a callback after every 5 characters are received */ FLEXCOM0_USART_ReadThresholdSet(5); /* Enable RX event notifications */ FLEXCOM0_USART_ReadNotificationEnable(true, false); while(1) { /* Wait until at-least 10 characters are entered by the user */ while (nBytesRead < 10); /* Echo the received data */ FLEXCOM0_USART_Write((uint8_t*)rxBuffer, nBytesRead); FLEXCOM0_USART_Write((uint8_t*)"\r\n>", 3); nBytesRead = 0; } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
SPI Mode
This section provides interface to use the FLEXCOM peripheral in SPI mode. The FLEXCOM SPI PLIB can be configured in master or slave mode.
SPI master mode
In SPI master mode, the PLIB can be configured to run in blocking mode or non-blocking mode. In blocking mode the peripheral interrupt is disabled and the transfer API blocks until the transfer is complete. In non-blocking mode, the peripheral interrupt is enabled. The transfer API initiates the transfer and returns immediately. The transfer is completed from the peripheral interrupt. Application can either use a callback to get notified when the transfer is complete or can use the IsBusy API to check the completion status.
SPI slave mode
SPI slave mode enables peripheral interrupt for data transfers. The PLIB uses internal receive and transmit buffers. The receive buffer is used to hold the data received from the SPI master while the application data to be transmitted out is copied into the transmit buffer. The size of the transmit and receive buffers is configurable in MCC. Application must register a callback with the PLIB to receive event notifications. A callback is given when the chip select is de-asserted by the SPI master. The application must read out the received data in the callback, thereby clearing the PLIB's internal RX buffer.
The PLIB optionally supports busy signalling from SPI slave to SPI master. This option can be enabled to provide an indication to the SPI master on when the SPI slave will be ready to respond. In a typical implementation, to read data from SPI slave, the SPI master asserts the chip select line and then sends a SPI packet informing the slave about the memory address to read from and the number of bytes to read and then de-asserts the chip select line. The SPI master must then wait for the SPI slave to frame the response by waiting on the busy line. Once the SPI slave drives the busy signal to ready state, the SPI master can start reading the actual data by asserting the chip select line and sending dummy writes for the number of bytes to read. Finally, after the intended bytes are read, the chip select must be de-asserted by the SPI master.
If the busy signalling is not enabled, the SPI master must wait for sufficient duration to allow the SPI slave to become ready with the response.
SPI Master in blocking (peripheral interrupt disabled) mode
// Following code demonstrates SPI self loopback with the PLIB configured in blocking mode uint8_t txData[] = "SELF LOOPBACK FOR SPI!"; uint8_t rxData[sizeof(txData)]; int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* SPI Write Read */ FLEXCOM0_SPI_WriteRead(&txData[0], sizeof(txData), &rxData[0], sizeof(rxData)); /* Compare received data with the transmitted data */ if ((memcmp(txData, rxData, sizeof(txData)) == 0)) { /* Pass: Received data is same as transmitted data */ } else { /* Fail: Received data is not same as transmitted data */ } while ( true ) { } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
SPI Master in non-blocking (peripheral interrupt enabled) mode
// Following code demonstrates SPI self loopback with the PLIB configured in non-blocking mode uint8_t txData[] = "SELF LOOPBACK FOR SPI!"; uint8_t rxData[sizeof(txData)]; volatile bool transferStatus = false; /* This function will be called by SPI PLIB when transfer is completed */ void APP_SPI_Callback(uintptr_t context ) { transferStatus = true; } int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Register callback function */ FLEXCOM0_SPI_CallbackRegister(APP_SPI_Callback, 0); /* SPI Write Read */ FLEXCOM0_SPI_WriteRead(&txData[0], sizeof(txData), &rxData[0], sizeof(rxData)); while (1) { /* Perform other tasks here ...*/ /* Check if transfer has completed */ if(transferStatus == true) { /* Compare received data with the transmitted data */ if(memcmp(txData, rxData, sizeof(txData)) == 0) { /* Pass: Received data is same as transmitted data */ } else { /* Fail: Received data is not same as transmitted data */ } } } }
SPI slave mode
This example uses the FLEXCOM SPI peripheral library in slave mode and allows reading and writing data from/to its internal buffer by a SPI master. The SPI master writes data by sending a write command followed by two bytes of memory address followed by the data to be written.
< WR_CMD > < ADDR_MSB > < ADDR_LSB > < DATA0 > ... < DATA n >
The SPI slave asserts the Busy line to indicate to the SPI master that it is busy. Once ready, the SPI slave de-asserts the Busy line. Once the SPI slave is ready, the SPI master reads the data by sending read command followed by two bytes of memory address and the number of bytes to read.
< RD_CMD > < ADDR_MSB > < ADDR_LSB > < NUM_BYTES >
The SPI slave responds by sending the data at the requested memory address.
typedef enum
{
APP_STATE_INITIALIZE,
APP_STATE_READ,
APP_STATE_WRITE,
APP_STATE_IDLE,
} APP_STATES;
/* Commands */
#define APP_CMD_WRITE 0x02
#define APP_CMD_READ 0x03
#define APP_MEM_BUFFER_SIZE 512
#define APP_RX_BUFFER_SIZE 256
#define APP_TX_BUFFER_SIZE 256
typedef struct
{
uint8_t busy :1;
uint8_t reserved :7;
}STATUS;
typedef struct
{
volatile APP_STATES state;
volatile STATUS status;
volatile uint8_t nBytesRead;
volatile uint8_t nBytesToWrite;
volatile uint8_t nBytesReadRequest;
volatile uint16_t memAddr;
}APP_DATA;
APP_DATA appData;
uint8_t APP_MemoryBuffer[APP_MEM_BUFFER_SIZE] =
{
0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f,
0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f,
0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f,
0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f,
0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f,
0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f,
0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,
0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f,
0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f,
0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f,
0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf,
0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf,
0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf,
0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf,
0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef,
0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff,
0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f,
0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f,
0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f,
0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f,
0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f,
0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f,
0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f,
0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f,
0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f,
0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f,
0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf,
0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf,
0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf,
0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf,
0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef,
0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff
};
uint8_t APP_RxData[APP_RX_BUFFER_SIZE];
uint8_t APP_TxData[APP_TX_BUFFER_SIZE];
void delay(uint32_t count)
{
uint32_t i;
// 1 loop roughly provides 1us delay at 32MHz CPU frequency
for (i = 0; i < count; i++)
{
asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");
asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");
asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");
asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");asm("NOP");
}
}
void SPIEventHandler(uintptr_t context )
{
if (FLEXCOM0_SPI_ErrorGet() == FLEXCOM_SPI_SLAVE_ERROR)
{
appData.nBytesRead = FLEXCOM0_SPI_Read(APP_RxData, FLEXCOM0_SPI_ReadCountGet());
switch(APP_RxData[0])
{
case APP_CMD_WRITE:
if (appData.status.busy == 0)
{
appData.status.busy = 1;
appData.memAddr = ((APP_RxData[1] << 8) | (APP_RxData[2]));
appData.nBytesToWrite = (appData.nBytesRead - 3);
appData.state = APP_STATE_WRITE;
}
break;
case APP_CMD_READ:
appData.memAddr = ((APP_RxData[1] << 8) | (APP_RxData[2]));
appData.nBytesReadRequest = APP_RxData[3];
if ((appData.memAddr + appData.nBytesReadRequest) <= APP_TX_BUFFER_SIZE)
{
memcpy(APP_TxData, &APP_MemoryBuffer[appData.memAddr], appData.nBytesReadRequest);
FLEXCOM0_SPI_Write(APP_TxData, appData.nBytesReadRequest);
}
break;
}
if (appData.status.busy == 0)
{
/* Indicate to SPI Master that slave is ready for data transfer */
FLEXCOM0_SPI_Ready();
}
}
}
int main ( void )
{
/* Initialize all modules */
SYS_Initialize ( NULL );
appData.state = APP_STATE_INITIALIZE;
while(1)
{
/* Check the application's current state. */
switch (appData.state)
{
case APP_STATE_INITIALIZE:
FLEXCOM0_SPI_CallbackRegister(SPIEventHandler, (uintptr_t) 0);
/* Wait for instructions from SPI master */
appData.state = APP_STATE_IDLE;
break;
case APP_STATE_WRITE:
/* Adding delay to simulate busy condition */
delay(1000);
/* Copy received data into Application memory buffer */
if ((appData.memAddr + appData.nBytesToWrite) <= APP_MEM_BUFFER_SIZE)
{
memcpy(&APP_MemoryBuffer[appData.memAddr], &APP_RxData[3], appData.nBytesToWrite);
}
appData.status.busy = 0;
appData.state = APP_STATE_IDLE;
/* Indicate to SPI Master that slave is ready for data transfer */
FLEXCOM0_SPI_Ready();
break;
case APP_STATE_IDLE:
break;
default:
break;
}
}
}TWI Mode
This section provides interface to use the FLEXCOM peripheral in TWI mode. The FLEXCOM TWI PLIB can be configured in master or slave mode.
TWI master mode
The FLEXCOM TWI peripheral library supports the following TWI transfers:
Master Write: The master writes a block of data to the slave Master Read: The master reads a block of data from the slave Master Write/Read: The master writes and then reads back a block of data from slave.
The block of data is transferred in a non-blocking manner using a peripheral interrupt. Application can either use a callback or IsBusy API to check for completion of data transfer.
TWI slave mode
TWI slave PLIB can be configured with peripheral interrupt enabled or disabled. When peripheral interrupt is enabled, application must register a callback, to get notified of the TWI events such as address match, transmitter ready, receiver ready etc. When peripheral interrupt is disabled, PLIB provides APIs to read the interrupt status flags. Application can call this API to determine the TWI event and then use the ReadByte/WriteByte APIs to read/write over the TWI bus.
TWI Master mode
// Following code demonstrates TWI write operation using polling method #define APP_SLAVE_ADDR 0x0057 #define NUM_BYTES 10 uint8_t myWriteData [NUM_BYTES] = {'1', '0', ' ', 'B', 'Y', 'T', 'E', 'S', '!', '!',}; int main(void) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Write data to the I2C Slave */ FLEXCOM0_TWI_Write(APP_SLAVE_ADDR, &myWriteData[0], NUM_BYTES); /* Poll and wait for the transfer to complete */ while(FLEXCOM0_TWI_IsBusy()); /* Check if any error occurred */ if(FLEXCOM0_TWI_ErrorGet() == FLEXCOM_TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } }
// Following code demonstrates TWI write operation using callback method #define APP_SLAVE_ADDR 0x0057 #define NUM_BYTES 10 uint8_t myWriteData [NUM_BYTES] = {'1', '0', ' ', 'B', 'Y', 'T', 'E', 'S', '!', '!',}; void FLEXCOM0_TWI_Callback(uintptr_t context) { if(FLEXCOM0_TWI_ErrorGet() == FLEXCOM_TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } } int main(void) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Register Callback function */ FLEXCOM0_TWI_CallbackRegister(FLEXCOM0_TWI_Callback, (uintptr_t)NULL); /* Submit Write Request */ FLEXCOM0_TWI_Write(APP_SLAVE_ADDR, &myWriteData[0], NUM_BYTES); }
TWI Slave mode
This example uses the TWI peripheral library in slave mode and emulates an EEPROM of 512 bytes. There are two pages each of size 256 bytes. TWI slave expects two bytes of memory address from the TWI master and the memory address can range from 0x00 to 0x1FF.
#define EEPROM_PAGE_SIZE_BYTES 256 #define EEPROM_PAGE_SIZE_MASK 0xFF #define EEPROM_SIZE_BYTES 512 typedef enum { EEPROM_CMD_WRITE, EEPROM_CMD_IDLE, }EEPROM_CMD; typedef struct { /* currentAddrPtr - to allow for sequential read (from the current address) */ uint16_t currentAddrPtr; /* addrIndex - used to copy 2 bytes of EEPROM memory address */ uint8_t addrIndex; /* wrBuffer - holds the incoming data from the TWI master */ uint8_t wrBuffer[EEPROM_PAGE_SIZE_BYTES]; /* wrBufferIndex - Index into the wrBuffer[] */ uint16_t wrBufferIndex; /* wrAddr - indicates the starting address of the EEPROM emulation memory to write to */ volatile uint16_t wrAddr; /* nWrBytes - indicates the number of bytes to write to EEPROM emulation buffer */ volatile uint8_t nWrBytes; /* internalWriteInProgress - indicates that EEPROM is busy with internal writes */ bool internalWriteInProgress; /* eepromCommand - used to trigger write to the EEPROM emulation buffer */ EEPROM_CMD eepromCommand; }EEPROM_DATA; EEPROM_DATA eepromData; uint8_t EEPROM_EmulationBuffer[EEPROM_SIZE_BYTES] = { 0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f, 0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f, 0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f, 0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f, 0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f, 0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f, 0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f, 0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f, 0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f, 0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f, 0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf, 0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf, 0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf, 0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf, 0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef, 0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff, 0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b,0x0c,0x0d,0x0e,0x0f, 0x10,0x11,0x12,0x13,0x14,0x15,0x16,0x17,0x18,0x19,0x1a,0x1b,0x1c,0x1d,0x1e,0x1f, 0x20,0x21,0x22,0x23,0x24,0x25,0x26,0x27,0x28,0x29,0x2a,0x2b,0x2c,0x2d,0x2e,0x2f, 0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x3a,0x3b,0x3c,0x3d,0x3e,0x3f, 0x40,0x41,0x42,0x43,0x44,0x45,0x46,0x47,0x48,0x49,0x4a,0x4b,0x4c,0x4d,0x4e,0x4f, 0x50,0x51,0x52,0x53,0x54,0x55,0x56,0x57,0x58,0x59,0x5a,0x5b,0x5c,0x5d,0x5e,0x5f, 0x60,0x61,0x62,0x63,0x64,0x65,0x66,0x67,0x68,0x69,0x6a,0x6b,0x6c,0x6d,0x6e,0x6f, 0x70,0x71,0x72,0x73,0x74,0x75,0x76,0x77,0x78,0x79,0x7a,0x7b,0x7c,0x7d,0x7e,0x7f, 0x80,0x81,0x82,0x83,0x84,0x85,0x86,0x87,0x88,0x89,0x8a,0x8b,0x8c,0x8d,0x8e,0x8f, 0x90,0x91,0x92,0x93,0x94,0x95,0x96,0x97,0x98,0x99,0x9a,0x9b,0x9c,0x9d,0x9e,0x9f, 0xa0,0xa1,0xa2,0xa3,0xa4,0xa5,0xa6,0xa7,0xa8,0xa9,0xaa,0xab,0xac,0xad,0xae,0xaf, 0xb0,0xb1,0xb2,0xb3,0xb4,0xb5,0xb6,0xb7,0xb8,0xb9,0xba,0xbb,0xbc,0xbd,0xbe,0xbf, 0xc0,0xc1,0xc2,0xc3,0xc4,0xc5,0xc6,0xc7,0xc8,0xc9,0xca,0xcb,0xcc,0xcd,0xce,0xcf, 0xd0,0xd1,0xd2,0xd3,0xd4,0xd5,0xd6,0xd7,0xd8,0xd9,0xda,0xdb,0xdc,0xdd,0xde,0xdf, 0xe0,0xe1,0xe2,0xe3,0xe4,0xe5,0xe6,0xe7,0xe8,0xe9,0xea,0xeb,0xec,0xed,0xee,0xef, 0xf0,0xf1,0xf2,0xf3,0xf4,0xf5,0xf6,0xf7,0xf8,0xf9,0xfa,0xfb,0xfc,0xfd,0xfe,0xff }; bool APP_FLEXCOM_TWI_Callback ( FLEXCOM_TWI_SLAVE_TRANSFER_EVENT event, uintptr_t contextHandle ) { bool isSuccess = true; switch(event) { case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_ADDR_MATCH: if ((FLEXCOM0_TWI_TransferDirGet() == FLEXCOM_TWI_SLAVE_TRANSFER_DIR_WRITE) && (eepromData.internalWriteInProgress == true)) { /* EEPROM is busy. Send NAK */ isSuccess = false; } else { /* Reset the indexes */ eepromData.addrIndex = 0; eepromData.wrBufferIndex = 0; } break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_RX_READY: /* Read the data sent by TWI Master */ if (eepromData.addrIndex < 2) { ((uint8_t*)&eepromData.currentAddrPtr)[eepromData.addrIndex++] = FLEXCOM0_TWI_ReadByte(); } else { eepromData.wrBuffer[(eepromData.wrBufferIndex & EEPROM_PAGE_SIZE_MASK)] = FLEXCOM0_TWI_ReadByte(); eepromData.wrBufferIndex++; } break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_TX_READY: /* Provide the EEPROM data requested by the TWI Master */ FLEXCOM0_TWI_WriteByte(EEPROM_EmulationBuffer[eepromData.currentAddrPtr++]); if (eepromData.currentAddrPtr >= EEPROM_SIZE_BYTES) { eepromData.currentAddrPtr = 0; } break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_STOP_BIT_RECEIVED: if (eepromData.wrBufferIndex > 0) { if (eepromData.wrBufferIndex > EEPROM_PAGE_SIZE_BYTES) { eepromData.wrBufferIndex = EEPROM_PAGE_SIZE_BYTES; } eepromData.wrAddr = eepromData.currentAddrPtr; eepromData.nWrBytes = eepromData.wrBufferIndex; /* Update the current address pointer to allow for sequential read */ eepromData.currentAddrPtr += eepromData.wrBufferIndex; /* Reset the indexes */ eepromData.addrIndex = 0; eepromData.wrBufferIndex = 0; /* Set busy flag to send NAK for any write requests */ eepromData.internalWriteInProgress = true; eepromData.eepromCommand = EEPROM_CMD_WRITE; } break; default: break; } return isSuccess; } void EEPROM_StateMachine(void) { switch(eepromData.eepromCommand) { case EEPROM_CMD_WRITE: memcpy(&EEPROM_EmulationBuffer[eepromData.wrAddr], &eepromData.wrBuffer[0], eepromData.nWrBytes); eepromData.internalWriteInProgress = false; eepromData.eepromCommand = EEPROM_CMD_IDLE; break; case EEPROM_CMD_IDLE: /* Do Nothing */ break; } } int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); eepromData.eepromCommand = EEPROM_CMD_IDLE; FLEXCOM0_TWI_CallbackRegister(APP_FLEXCOM_TWI_Callback, 0); while ( true ) { EEPROM_StateMachine(); } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
Library Interface
FLEXCOM peripheral library provides the following interfaces:
USART Mode
Functions
| Name | Description | Blocking mode | Non-blocking mode | Ring buffer mode |
|---|---|---|---|---|
| FLEXCOMx_USART_Initialize | Initializes given instance of the USART peripheral | Yes | Yes | Yes |
| FLEXCOMx_USART_SerialSetup | Sets up serial configurations for USART peripheral | Yes | Yes | Yes |
| FLEXCOMx_USART_Write | Writes data to the given USART peripheral instance | Yes | Yes | Yes |
| FLEXCOMx_USART_Read | Reads data from the given USART peripheral instance | Yes | Yes | Yes |
| FLEXCOMx_USART_WriteIsBusy | Returns the write request status associated with the given USART peripheral instance | No | Yes | No |
| FLEXCOMx_USART_ReadIsBusy | Returns the read request status associated with the given USART peripheral instance | No | Yes | No |
| FLEXCOMx_USART_WriteCountGet | Gets the byte count of processed bytes for a given USART read operation in non-blocking mode. Returns the number of bytes pending to be transmitted out in the transmit buffer in ring buffer mode. | No | Yes | Yes |
| FLEXCOMx_USART_ReadCountGet | Gets the byte count of processed bytes for a given USART read operation in non-blocking mode. Returns the number of bytes available in the internal receive buffer of the PLIB in ring buffer mode. | No | Yes | Yes |
| FLEXCOMx_USART_TransmitterIsReady | Returns the hardware status of the USART Transmitter | Yes | No | No |
| FLEXCOMx_USART_ReceiverIsReady | Returns the hardware status of the USART Receiver | Yes | No | No |
| FLEXCOMx_USART_ErrorGet | Gets the error of the given USART peripheral instance | Yes | Yes | Yes |
| FLEXCOMx_USART_WriteCallbackRegister | Sets the pointer to the function (and it's context) to be called when the given USART's write events occur | No | Yes | Yes |
| FLEXCOMx_USART_ReadCallbackRegister | Sets the pointer to the function (and it's context) to be called when the given USART's read events occur | No | Yes | Yes |
| FLEXCOMx_USART_ReadByte | Submits request to read a byte of data to the given USART peripheral | Yes | No | No |
| FLEXCOMx_USART_WriteByte | Submits a byte of data to the given USART peripheral to transfer | Yes | No | No |
| FLEXCOMx_USART_ReadAbort | Aborts the ongoing read request | No | Yes | No |
| FLEXCOMx_USART_WriteFreeBufferCountGet | Returns the number of bytes of free space available in the internal transmit buffer | No | No | Yes |
| FLEXCOMx_USART_WriteBufferSizeGet | Returns the size of the internal transmit ring buffer | No | No | Yes |
| FLEXCOMx_USART_WriteNotificationEnable | This API lets the application turn the transmit notifications on/off | No | No | Yes |
| FLEXCOMx_USART_WriteThresholdSet | This API allows the application to set a threshold level on the number of free space available in the transmit buffer | No | No | Yes |
| FLEXCOMx_USART_ReadFreeBufferCountGet | Returns the number of bytes of free space available in the internal receive buffer | No | No | Yes |
| FLEXCOMx_USART_ReadBufferSizeGet | Returns the size of the receive ring buffer | No | No | Yes |
| FLEXCOMx_USART_ReadNotificationEnable | This API lets the application turn the receive notifications on/off | No | No | Yes |
| FLEXCOMx_USART_ReadThresholdSet | This API allows the application to set a threshold level on the number of bytes of data available in the receive buffer | No | No | Yes |
| FLEXCOMx_USART_IrDA_DirectionSet | Sets the data transfer direction in IRDA mode | Yes | Yes | No |
Data types and constants
| Name | Type | Description | Blocking mode | Non-blocking mode | Ring buffer mode |
|---|---|---|---|---|---|
| FLEXCOM_USART_ERROR | Macros and Typedef | Defines the macros and typedefs associated with the USART peripheral errors | Yes | Yes | Yes |
| FLEXCOM_USART_DATA | Enum | Defines the data width types for the USART peripheral | Yes | Yes | Yes |
| FLEXCOM_USART_PARITY | Enum | Defines the parity types for the USART peripheral | Yes | Yes | Yes |
| FLEXCOM_USART_STOP | Enum | Defines the data type for the USART peripheral stop bits | Yes | Yes | Yes |
| FLEXCOM_USART_SERIAL_SETUP | Struct | Defines the data structure which is used to configure USART serial parameters at run time | Yes | Yes | Yes |
| FLEXCOM_USART_CALLBACK | Typedef | Defines the data type and function signature of the USART peripheral library callback function | Yes | Yes | No |
| FLEXCOM_USART_EVENT | Enum | Defines the enums associated with the USART events in the ring buffer mode | Yes | Yes | Yes |
| FLEXCOM_USART_RING_BUFFER_CALLBACK | Typedef | Defines the data type and function signature for the FLEXCOM_USART peripheral callback function in the ring buffer mode | No | No | Yes |
| FLEXCOM_IRDA_DIR | Enum | Defines the data type for IRDA direction | Yes | Yes | No |
SPI Mode
Functions
| Name | Description | Master (blocking/interrupt disabled) mode | Master (non-blocking/interrupt enabled) mode | Slave mode |
|---|---|---|---|---|
| FLEXCOMx_SPI_Initialize | Initializes instance x of the FLEXCOM module operating in SPI master or slave mode | Yes | Yes | Yes |
| FLEXCOMx_SPI_TransferSetup | Configure FLEXCOM SPI operational parameters at run time | Yes | Yes | No |
| FLEXCOMx_SPI_WriteRead | Write and Read data on FLEXCOM SPI peripheral | Yes | Yes | No |
| FLEXCOMx_SPI_Write | Writes data to FLEXCOM x SPI peripheral | Yes | Yes | Yes |
| FLEXCOMx_SPI_Read | Reads data on the FLEXCOM SPI peripheral in SPI master mode. Reads data from the PLIB's internal buffer to the application buffer in SPI slave mode | Yes | Yes | Yes |
| FLEXCOMx_SPI_CallbackRegister | Allows application to register a callback with the PLIB | No | Yes | Yes |
| FLEXCOMx_SPI_IsBusy | Returns transfer status of FLEXCOM SPI | No | Yes | Yes |
| FLEXCOMx_SPI_ReadCountGet | Returns the number of bytes pending to be read out from the PLIB's internal buffer | No | No | Yes |
| FLEXCOMx_SPI_ReadBufferSizeGet | Returns the size of the PLIB's internal receive buffer | No | No | Yes |
| FLEXCOMx_SPI_WriteBufferSizeGet | Returns the size of the PLIB's internal transmit buffer | No | No | Yes |
| FLEXCOMx_SPI_ErrorGet | Returns the error status of SPI transfer | No | No | Yes |
| FLEXCOMx_SPI_Ready | Drives the SPI slave busy line to ready (not busy) state | No | No | Yes |
Data types and constants
| Name | Description | Master (blocking/interrupt disabled) mode | Master (non-blocking/interrupt enabled) mode | Slave mode |
|---|---|---|---|---|
| FLEXCOM_SPI_CLOCK_PHASE | Enum | Identifies SPI Clock Phase Options | Yes | Yes |
| FLEXCOM_SPI_CLOCK_POLARITY | Enum | Identifies SPI Clock Polarity Options | Yes | Yes |
| FLEXCOM_SPI_DATA_BITS | Enum | Identifies SPI bits per transfer | Yes | Yes |
| FLEXCOM_SPI_CHIP_SELECT | Enum | Enumerator constants for SPI hardware chip select | Yes | Yes |
| FLEXCOM_SPI_TRANSFER_SETUP | Struct | Data structure containing the SPI parameters which can be changed at run time | Yes | Yes |
| FLEXCOM_SPI_CALLBACK | Typedef | Defines the data type and function signature for the FLEXCOM SPI peripheral callback function | No | Yes |
| FLEXCOM_SPI_SLAVE_ERROR | Macros and Typedef | Defines the macros and typedef associated with SPI slave mode errors | No | No |
| FLEXCOM_SPI_SLAVE_CALLBACK | Typedef | Pointer to a SPI Call back function when SPI is configued in slave mode | No | No |
TWI Mode
Functions
| Name | Description | Master mode | Slave mode (interrupt disabled) | Slave mode (interrupt enabled) |
|---|---|---|---|---|
| FLEXCOMx_TWI_Initialize | Initializes the instance of the FLEXCOM peripheral in either master or slave mode | Yes | Yes | Yes |
| FLEXCOMx_TWI_Read | Reads data from the slave | Yes | No | No |
| FLEXCOMx_TWI_Write | Writes data to the slave | Yes | No | No |
| FLEXCOMx_TWI_WriteRead | Write and Read data from Slave | Yes | No | No |
| FLEXCOMx_TWI_IsBusy | Returns the Peripheral busy status | Yes | No | Yes |
| FLEXCOMx_TWI_ErrorGet | Returns the TWI error that occurred on the bus | Yes | Yes | Yes |
| FLEXCOMx_TWI_TransferSetup | Dynamic setup of TWI Peripheral | Yes | No | No |
| FLEXCOMx_TWI_CallbackRegister | Sets the pointer to the function (and it's context) to be called when the given FLEXCOM TWI's transfer events occur | Yes | No | Yes |
| FLEXCOMx_TWI_StatusGet | Returns the TWI hardware status flags | No | Yes | No |
| FLEXCOMx_TWI_ReadByte | Read the received TWI byte | No | Yes | Yes |
| FLEXCOMx_TWI_WriteByte | Write a data byte to TWI master | No | Yes | Yes |
| FLEXCOMx_TWI_TransferDirGet | Returns the TWI transfer direction | No | Yes | Yes |
| FLEXCOMx_TWI_LastByteAckStatusGet | Returns the ACK status of the last byte written to the TWI master | No | Yes | Yes |
| FLEXCOMx_TWI_NACKDataPhase | Configures the hardware to send ACK or NAK for the next byte that will be received from the TWI master | No | Yes | Yes |
Data types and constants
| Name | Type | Description | Master mode | Slave mode (interrupt disabled) | Slave mode (interrupt enabled) |
|---|---|---|---|---|---|
| FLEXCOM_TWI_ERROR | Enum | Defines the possible errors that the FLEXCOM TWI peripheral can generate in TWI master mode | Yes | No | No |
| FLEXCOM_TWI_TRANSFER_SETUP | Struct | TWI transfer setup data structure | Yes | No | No |
| FLEXCOM_TWI_CALLBACK | Typedef | Defines the data type and function signature for the FLEXCOM TWI peripheral callback function in TWI master mode | Yes | No | No |
| FLEXCOM_TWI_SLAVE_TRANSFER_DIR | Enum | Defines the enum for TWI data transfer direction | No | Yes | Yes |
| FLEXCOM_TWI_SLAVE_ACK_STATUS | Enum | Defines the enum for the TWI acknowledgement | No | Yes | Yes |
| FLEXCOM_TWI_SLAVE_STATUS_FLAG | Enum | Defines the list of possible TWI slave events | No | Yes | No |
| FLEXCOM_TWI_SLAVE_TRANSFER_EVENT | Enum | Defines the enum for the TWI slave transfer event | No | No | Yes |
| FLEXCOM_TWI_SLAVE_CALLBACK | Typedef | Defines the data type and function signature for the FLEXCOM TWI Slave callback function | No | No | Yes |