2.49.6 GENERIC_TIMER_PeriodSet Function
C
void GENERIC_TIMER_PeriodSet(uint64_t period);
Summary
Set the timer period value.
Description
This function sets the timer period value.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| period | The period value of generic timer. For example, if the timer is running at a frequency of 24 MHz and if the desired timeout is 10 milliseconds, then the period value must be specified as 24MHz x (10/1000) = 240000 cycles |
Returns
None.