4.6.44.6.11 USB_CDC_NOTIFICATION_ID_enum
enum USB_CDC_NOTIFICATION_ID_enum
| USB_CDC_NOTIFICATION_NETWORK_CONNECTION |
Notifies the host about network connection status |
| USB_CDC_NOTIFICATION_RESPONSE_AVAILABLE |
Notifies the host that a response is available |
| USB_CDC_NOTIFICATION_AUX_JACK_HOOK_STATE |
Indicates that the loop has changed on the auxiliary phone interface of the USB device |
| USB_CDC_NOTIFICATION_RING_DETECT |
Indicates ring voltage on the POTS line interface of the USB device |
| USB_CDC_NOTIFICATION_SERIAL_STATE |
Sends asynchronous notification of UART status |
| USB_CDC_NOTIFICATION_CALL_STATE_CHANGE |
Identifies that a change has occurred to the state of a call on the line corresponding to the interface or union for the line |
| USB_CDC_NOTIFICATION_LINE_STATE_CHANGE |
Identifies that a change has occurred to the state of the line corresponding to the interface or main interface of a union sending the notification message |
| USB_CDC_NOTIFICATION_CONNECTION_SPEED_CHANGE |
Informs the host-networking driver that a change in either the uplink or the downlink bit rate of the connection has occurred |
| USB_CDC_NOTIFICATION_MDML_SEMANTIC_MODEL_SPECIFIC_NOTIFICATION |
Notification code 40h-5Fh for MDLM Semantic-Model specific notifications |