13.5.1 Overview
Depending on the application, peripherals may require specific clock frequencies to operate correctly. The Generic Clock controller GCLK provides nine Generic Clock Generators [8:0] that can provide a wide range of clock frequencies.
Generators can be set to use different external and
internal oscillators as source. The clock of each Generator can be divided. The outputs
from the Generators are used as sources for the Peripheral Channels, which provide the
Generic Clock (GCLK_PERIPH) to the peripheral modules, as shown in Figure 13-13. The number of Peripheral Clocks depends on how many
peripherals the device has.
Note: The
Generator 0 is always the direct source of the GCLK_MAIN signal.