Case 2: Secure SAM-BA Monitor is still available (the “MON_DIS” word is zeroed in the Boot Configuration Packet - not recommended for systems in production)
- Disable the access to the external boot memory (Chip Select pin, Card Detect pin, etc., depending on the chosen boot memory) to prevent its access by the ROM code on the next reboot.
- Connect a USB cable on the USB device port, or on the UART used as SAM-BA Monitor console terminal.
- Reset the chip.
- Enable access to the external boot memory.
- Program the bootstrap using the SAM-BA tool.