7.8.2.6 Application Code End

The default value given in this fuse description is the factory-programmed value and should not be mistaken for the Reset value.
Name: APPEND
Offset: 0x07
Reset: 0x00
Property: -

Bit 76543210 
 APPEND[7:0] 
Access RRRRRRRR 
Reset 00000000 

Bits 7:0 – APPEND[7:0] Application Code Section End

These bits set the end of the application code section in blocks of 256 bytes. The end of the application code section should be set as the BOOT size plus application code size. The remaining Flash will be application data. A value of 0x00 defines the Flash from BOOTEND*256 to the end of Flash as the application code section. When FUSE.BOOTEND is 0x00, the entire Flash is the BOOT section.