6.2 Stream Format

The data stream Stream Format is processed in the same order as the variables specified in the Variable Streamer. All data must be given as little endian values, meaning that the lowest byte must be sent first. Additionally, a wrapper consisting of one byte before and one byte after the data stream variables must be added. This wrapper is used by the interpreter to synchronize to the data stream. The start byte can be of an arbitrary but the end byte must be the inverse of the Start byte. The start and end bytes are not defined in the configuration.

The figure below gives an example raw data transmission where ADC0 is 185, ADC1 is 950, ADC2 is 0, and Prescaler is 2.
Figure 6-1. Data Streamer